VDD_xxx_IN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VDD_xxx_IN

455 Views
eishishibusawa
Contributor III

Dear Sir

 

I want to ask about the VDD_ARM_IN and VDD_SOC_IN of i.MX6Dual.

I understand that there is the following merit when dividing the power supply of VDD_ARM_IN and VDD_SOC_IN.

It is able to reduce the power consumption by setting an appropriate voltage for each.

 

Q1.

Are there any problem when it is not separated the power supply for VDD_ARM_IN and VDD_SOC_IN.

 

Best Regards,

Eishi SHIBUSAWA

Labels (1)
0 Kudos
Reply
1 Reply

361 Views
Yuri
NXP Employee
NXP Employee

Hello,

  VDD_ARM_IN and VDD_SOC_IN may be supplied from the same source,

assuming the supply can provide proper current load / capacity.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply