VDD_HIGH_IN question in Rev. 7, 10/2016 datasheet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VDD_HIGH_IN question in Rev. 7, 10/2016 datasheet

1,405 Views
MaxChou
Contributor III

Dear  Sir

my customer has a old design, they using PF0100 Vgen6(3.3V) for VDD_HIGH_IN,

but latest datasheet, add VDD_HIGH_IN max value is 2.85V in LDO bypass mode,

未命名.png

Table 8. Operating Ranges

未命名1.png

this info let them so confuse,

but they can't modify H/W in current status,

could they keep original design ?

or they could to modify vgen6 output in u-boot/kernel ?

 

Max

Labels (2)
0 Kudos
Reply
3 Replies

1,284 Views
art
NXP Employee
NXP Employee

This is the typo in the documentation since the VDD_HIGH regulator just doesn't have the bypass mode. Just ignore it.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,284 Views
RossMcLuckie
NXP Employee
NXP Employee

Hi Max,

I'm checking this for you and will try to confirm shortly, but I believe this is an error in our doc update. The regulators associated with VDD_HIGH_IN do not support bypass mode, so there is no need for the LDO bypass definition and you should be able to ignore this.

I will confirm this ASAP and if I am correct we will look to correct this in the next doc update.

Regards

Ross

0 Kudos
Reply

1,284 Views
RossMcLuckie
NXP Employee
NXP Employee

Hi,

Just to confirm this is indeed a documentation error that you can ignore until we update the document and remove the incorrect "VDD_HIGH_IN supply voltage (LDO bypass entries)".

Regards

Ross

0 Kudos
Reply