The AN4397.pdf application note regarding common hardware for i.MX6 Solo, Duallite, Dual & Quad, says,
The third difference is about VDD_CACHE_CAP (N12). In i.MX 6Quad and i.MX 6Dual,
VDD_CACHE_CAP should be connected to VDDSOC_CAP, whereas in i.MX 6DualLite and
i.MX 6Solo, pin N12 can be NC.
Is it is OK to keep the N12 Pad connected to VDDSOC_CAP power supply for Duallite also, or whether it has to be mandatorily NC for Duallite & Solo ?
Hi Sree,
Did you got the answer for the question posted. I am also looking for it.
Thanks,
Karthik R
Hi Karthik,
I haven't got clarity on this yet. However I am following the SABREBOARD design, in which the VDDSOC_CAP is kept connected to the NC_N12 for Duallite version as well. Fingers Xed !!!