VAR-SOM-MX6: It is possible to install chromium browser on the Variscite VAR-SOM-MX6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VAR-SOM-MX6: It is possible to install chromium browser on the Variscite VAR-SOM-MX6?

1,993 Views
ferranselva
Contributor I

Hello,

I have a variscite VAR-SOM-MX6 (VSM-M6-501) board, and I want to install the chromium browser on the Yocto OS.

I don't know if this is possible, in afirmative case, if you know a manual, to do this, can you provide it?

Perhaps, somebody has made this before, it is possible to get the binary files of the browser?

Thanks

Ferran.

Labels (3)
0 Kudos
Reply
2 Replies

1,293 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ferran

please look at link below

Porting Chrome on i.mx6 with hw accelaration?

I think you can ask on that link for more details

or meta-fsl-arm mailing list.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,293 Views
ferranselva
Contributor I

Thanks Chipexpert!

0 Kudos
Reply