Hi,
I am trying to use the VADC at the MX6SX SDB. (i.MX L3.14.52_1.1.0 GA)
I connected the camera input at the VADC_IN0, and I checked the signal after the C353 using the oscilloscope, and it is okay.

The imx6sx-sdb.dts says:
&vadc {
vadc_in = <0>;
csi_id = <1>;
status = "okay";
port {
vadc_ep: endpoint {
remote-endpoint = <&csi2_ep>;
};
};
};
The i.MX_Linux_Reference_Manual says:

My unit_tests doesn't have "csi_v4l2_tvin.out"
root@imx6sxsabresd:/unit_tests# ls
all-suite.txt check_mixer.out mxc_l2switch_test.out
audio8k16S.wav check_recording.out mxc_mcc_tty_test.out
autorun-asrc.sh check_synchronization.out mxc_mlb_test.out
autorun-ata.sh check_volume2.out mxc_sdma_test.out
autorun-fb.sh csi_v4l2_overlay.out mxc_spdc_fb_test.out
autorun-firi.sh daisy-640x480-565.rgb mxc_spi_test1.out
autorun-hantro.sh dbg_monitor.sh mxc_tuner_test.out
autorun-keypad.sh desk240x180-565.rgb mxc_tuner_test.sh
autorun-mmc-blockrw.sh dryice.sh mxc_tve_test.sh
autorun-mmc-fdisk.sh dump-clocks-dot.sh mxc_uart_stress_test.out
autorun-mmc-fs.sh dump-clocks.sh mxc_uart_test.out
autorun-mmc-mkfs.sh etm mxc_uart_xmit_test.out
autorun-mmc.sh gpu.sh mxc_v4l2_output.out
autorun-mxc_uart.sh gpuinfo.sh mxc_v4l2_still.out
autorun-oprofile.sh memtool mxc_v4l2_tvin.out
autorun-owire.sh mmdc2 pansy-1280x720-565.rgb
autorun-pxp.sh mx6s_v4l2_capture.out plumbago-1280x1024-565.rgb
autorun-rtc.sh mxc_asrc_test.out pxp_test.out
autorun-sound.sh mxc_dcic_test.out pxp_v4l2_out_test.sh
autorun-usb-gadget.sh mxc_epdc_fb_test.out pxp_v4l2_test.out
autorun-usb-host.sh mxc_epdc_v2_fb_test.out rose-800x600-565.rgb
autorun-v4l2.sh mxc_epdc_x11_fb_test.out rtctest.out
autorun-wdog.sh mxc_fb_test.out rtcwakeup.out
autorun.sh mxc_fb_vsync_test.out suspend_quick_auto.sh
cam2mpeg4.out mxc_i2c_slave_test.out suspend_random_auto.sh
check_2w1r.out mxc_iim_test.out test-utils.sh
check_audio.out mxc_irlan_test.sh wall-1024x768-565.rgb
check_ioctls.out mxc_isl29023.out wdt_driver_test.out
check_minor_open.out mxc_keyb_test.sh x11_overlay.out
Some debugs:
/**********************************************************************************************/
root@imx6sxsabresd:/unit_tests# lsmod
Module Size Used by
mx6s_capture 14549 0
mxc_dcic 6569 0
ov5640_camera 20096 0
evbug 1875 0
/**********************************************************************************************/
root@imx6sxsabresd:/unit_tests# ./mx6s_v4l2_capture.out -l
open video device /dev/video0
Video device /dev/video0 not support v4l2 capture
open video device /dev/video1
Found v4l2 capture device /dev/video1
open video device /dev/video2
Found v4l2 capture device /dev/video2
unable to open /dev/video3 for capture device.
unable to open /dev/video4 for capture device.
/**********************************************************************************************/
root@imx6sxsabresd:/unit_tests# ./mxc_v4l2_tvin.out -ow 1024 -oh 768
Unable to open /dev/video17
/**********************************************************************************************/
How can I test the camera input?
Thanks.