VADC & IMX6SX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

VADC & IMX6SX

1,387 次查看
mirkoardinghi1
Contributor IV

Hi

I'm using imx6sx with fido (kernel 3.14.28)

when I launch:

gst-launch-1.0 imxv4l2src device=/dev/video1 ! imxv4l2sink device=/dev/video0

I have a  lots of

mx6s-csi 221c000.csi: 86900000 != 86b00000

mx6s-csi 221c000.csi: 86b00000 != 87300000

mx6s-csi 221c000.csi: 86d00000 != 86f00000

mx6s-csi 221c000.csi: 86f00000 != 87100000

mx6s-csi 221c000.csi: 87100000 != 86700000

mx6s-csi 221c000.csi: 86700000 != 86900000

....

and the image (on the video0) is wrong

If I interrupt the gst-launch the memory is corrupted

-sh: /usr/bin/free: Accessing a corrupted shared library

-sh: symbol lookup error: /lib/libc.so.6: undefined symbol: __tls_get_addr, version GLIBC_2.4

Any help?

标签 (3)
标记 (3)
0 项奖励
回复
1 回复

1,045 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Mirko,

It is recommended trying with the most recent Linux release. You could take a look at L4.1.15_1.0.0_iMX6SX BSP.

Additionally, the following thread could provide useful information:

iMX6SX: VADC: force video standard

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复