V4l2h264dec is not available in Google coral

cancel
Showing results for 
Search instead for 
Did you mean: 

V4l2h264dec is not available in Google coral

271 Views
Manikandan
Contributor II

Hi ,

We are trying to receive rtsp video streams with i.MX 8M based boards

when we tried with iMX8MQ EVK Board and iMX8M Mini EVK Board we are getting maximum 24 FPS

but when we try with Google coral board we are getting   8 FPS  Only

Once I debug this i got to know that  iMX8MQ EVK Board and iMX8M Mini EVK Board  OS's using V4l2H264DEC whereas Google coral using VPUDEC

will it be the issue ?

if so i have tried installing V4l2H264DEC plugin in Google Coral's Mendel OS, but i wasn't able to achieve it. can anyone suggest me how to do it ?

The pipeline which we are using :

gst-launch-1.0 rtspsrc location=rtsp://10.0.0.1:9098/stream latency=0 connection-speed=30000 user-id=client  user-pw=password ! queue ! decodebin ! queue ! videoconvert ! autovideosink
 
 

 

Tags (3)
0 Kudos
3 Replies

252 Views
Manikandan
Contributor II

Thank you for the response.

Actually the mendel os doesn't have v4l2h264dec. i'm in the process of adding it. can you tell me any way to add this v4l2h264dec plugin

0 Kudos

256 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Manikanban,

Is the VPUDEC usage, you can tell mendel OS to change the pipeline to v4l2h264dec for better perfomance.

 

Regards

0 Kudos

207 Views
Manikandan
Contributor II

Thank you for the response @Bio_TICFSL 

In the mendel os we have to install gstreamer explicitly in that installation  v4l2h264dec or  imxvpudec  not there. can you please help me how can i add any one of these hardware decoder

Thank you

0 Kudos