Using uuu_imx_android_flash.bat to download image hanging issue on iMX8M_Nano

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using uuu_imx_android_flash.bat to download image hanging issue on iMX8M_Nano

1,056 次查看
sam_liu
Contributor II

Hi Sirs,

  The hardware of my customer board is iMX8M Nano with a 512MB DDR4, and I'm trying to porting Android 11 on it.

  I using "Android 11.0.0_2.0.0 (Linux 5.10.9 kernel)" BSP as the code base to porting new parameters  correspond to my customer board's DDR 4.

  After compiled the images successfully,  I using  "uuu_imx_android_flash.bat"  to download image on Win 10.

 When I type in the download command :  .\uuu_imx_android_flash.bat -f imx8mn -a -u ddr4 -d ddr4 -e 

it always stop(or stuck) at the status shown as below:

 

1:102 1/ 1 [=================100%=================] SDPS: boot -f u-boot-imx8mn-ddr4-evk-uuu.imx.link

uuufail.jpg

Could you please guide me how to fix it?

Is there a more detailed log about this tool can be checked? 

Waiting for your kind response, Thank you in advance.

  

0 项奖励
回复
0 回复数