Using the i.MX53 UART CTS signal for automatic transmission control.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the i.MX53 UART CTS signal for automatic transmission control.

Jump to solution
906 Views
mmichaelis
Contributor I
Can the UART on the i.MX53 use the CTS signal to automatically enable when transmitting and disable at the end of transmission.This would be useful for doing half-duplex RS-485 communications.
Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
705 Views
igorpadykov
NXP Employee
NXP Employee

Hi mmichaelis

unfortunatey not, i.MX53 UART does not fully support RS485 mode

(in particular direction control), opposite to i.MX6 UART, which supports that.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
706 Views
igorpadykov
NXP Employee
NXP Employee

Hi mmichaelis

unfortunatey not, i.MX53 UART does not fully support RS485 mode

(in particular direction control), opposite to i.MX6 UART, which supports that.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply