Using qt in I.MX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,901件の閲覧回数
JHY
Contributor IV

I.MX6UL has no accelerator for 2D/3D.

Does it mean that I.MX6UL can't use QT applications at all?

ラベル(1)
タグ(1)
1 解決策
2,449件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

in general it can use as discussed on meta-fsl-arm mailing list:

Freescale OpenEmbedded/Yocto Layers discussion list ()

however it is not supported in official bsp, refer to attached Release Notes p.8.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,450件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

in general it can use as discussed on meta-fsl-arm mailing list:

Freescale OpenEmbedded/Yocto Layers discussion list ()

however it is not supported in official bsp, refer to attached Release Notes p.8.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------