Hello Guys,
I'm using a sabresd board which is running linux and on top of that my console based application.
The application crashes at some point.
Is it possible to attached lauterbach debugger with trace32 software after the crash is observed? It should not reset the board. Moreover, the debugger was not at all attached when the board was powered on.
If this is possible, can someone help me with cmm script to be used for sabresd board (or in last case, imx6 chip)?
Thanks,
Urvish.
Solved! Go to Solution.
Hi Urvish
please check debug scripts included in ddr tester package on
https://community.freescale.com/docs/DOC-105652
and AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello igorpadykov,
Thank you for the quick reply.
I have gone through both the links throughly. I see a scripts under ddr tester package but they are not for lauterbach debugger. Moreover, it has more to do to with ddr test then pluggin in the debugger on live crashed board.
AN4553 has been a knowledge improver for sure but still didn't help me with lauterbach debugger scripts.
Thanks,
Urvish
Hello Igor,
Sorry for the delayed reply.
I saw this files earlier also from another post on the forum and did try that but it failed. I guess it was due to usage of non supported debug probe on lauterbach.
Thanks for the pointer. It forced me to check the probe and verify that I need to change it.
Regards,
Urvish