Using l5.1.1_2.0.0_6qp-ga binaries in a kk4.4.3_2.0.0-ga

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using l5.1.1_2.0.0_6qp-ga binaries in a kk4.4.3_2.0.0-ga

1,747 次查看
DiegoFSL
Contributor III

Hi i.MX Community,

with our software we're experiencing random system freezes (due to GPU lockup) in kk4.4.3_2.0.0-ga that happen generally after 1 to 3 days of continuous run on a Boundary Devices Nitrogen6X.

The source of the problem seems to be in hwcomposer: removing all /system/lib/hw/hwc* libraries fixes the problem, but reduces graphical performance too.

We've tried using hwcomposer_fsl.imx6.so and hwcomposer_viv.imx6.so from l5.0.0_1.0.0-ga, but same problem holds.

We've tried also using hwcomposer_fsl.imx6.so and hwcomposer_viv.imx6.so from l5.1.1_2.0.0_6qp-ga and that fixes the lockup problem and brings also the performance we desire.

Problem is that the l5.1.1_2.0.0_6qp-ga is a i.MX6 Quad Plus only release. Even if we acknowledge hwcomposer_fsl.imx6.so and hwcomposer_viv.imx6.so from l5.1.1_2.0.0_6qp-ga are not meant to be used with i.MX6Q, are we allowed to use those files inside a kk4.4.3_2.0.0-ga release from a license standpoint?

Thanks,

Diego

1 回复

918 次查看
gary_bisson
Senior Contributor III

Hi Diego,

A new release of KitKat (KK4.4.3_2.0.1) has been made by NXP to update the graphics libraries:

IMX6_KK443_201_ANDROID_SOURCE_BSP

http://www.nxp.com/webapp/Download?colCode=IMX6_KK443_201_ANDROID_DOCS

Hope this helps.

Regards,

Gary