Using iMX6 Solo and DDR3 - are both diff clock pairs DRAM_SDCLK_0 and DRAM_SDCLK_1 active in the Solo part?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using iMX6 Solo and DDR3 - are both diff clock pairs DRAM_SDCLK_0 and DRAM_SDCLK_1 active in the Solo part?

1,041件の閲覧回数
psayles
Contributor I

Using iMX6 Solo and DDR3 - are both diff clock pairs DRAM_SDCLK_0 and DRAM_SDCLK_1 active in the Solo part?

ラベル(3)
0 件の賞賛
返信
1 返信

799件の閲覧回数
Yuri
NXP Employee
NXP Employee

Generally signals CS0, ODT0, SDCKE0 relate to the CS0 channel ; signals CS1,

ODT1, SDCKE1 relate to the CS1 channel.

Clock signals SDCLK0 and SDCLK1 in default state are the same and can be used

for both CS0 or CS1 channels if this makes easier PCB design.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信