Hi,
I try to use ecspi5 on the i.MX6soloX board.
&flexcan1 { &flexcan2 { &qspi1 { &qspi2 { &ecspi5 { #if 0 spi-slave; #endif &iomuxc { |
1. question. spi devices are not retrieved on /dev. How do I create it?
| root@imx6sxsabresd:~# ls -al /dev/spi* ls: cannot access '/dev/spi*': No such file or directory root@imx6sxsabresd:~# dmesg | grep spi [ 1.054004] spi_imx 228c000.ecspi: dma setup error -19, use pio [ 1.058943] spi_imx 228c000.ecspi: probed root@imx6sxsabresd:~# ls -al /sys/bus/platform/drivers/spi_imx/228c000.ecspi lrwxrwxrwx 1 root root 0 Jun 23 08:35 /sys/bus/platform/drivers/spi_imx/228c000.ecspi -> ../../../../devices/soc0/soc/2200000.aips-bus/228c000.ecspi root@imx6sxsabresd:~# ls -al /sys/devices/soc0/soc/2200000.aips-bus/228c000.ecspi total 0 drwxr-xr-x 4 root root 0 Jun 23 07:48 . drwxr-xr-x 13 root root 0 Jun 23 07:48 .. lrwxrwxrwx 1 root root 0 Jun 23 08:35 driver -> ../../../../../bus/platform/drivers/spi_imx -rw-r--r-- 1 root root 4096 Jun 23 08:35 driver_override -r--r--r-- 1 root root 4096 Jun 23 08:35 modalias lrwxrwxrwx 1 root root 0 Jun 23 08:35 of_node -> ../../../../../firmware/devicetree/base/soc/aips-bus@02200000/ecspi@0228c000 drwxr-xr-x 2 root root 0 Jun 23 08:34 power drwxr-xr-x 3 root root 0 Jun 23 07:48 spi_master lrwxrwxrwx 1 root root 0 Jun 23 07:48 subsystem -> ../../../../../bus/platform -rw-r--r-- 1 root root 4096 Jun 23 07:48 uevent root@imx6sxsabresd:~# |
2. question. What value should each pin set on iomuxc? (there is no xml for i.mx6sx in iomuxtool)
3. question. How do I change to slave mode? Is there anything else I need to add besides "spi-slave;"?
4. question. Can I get the *.mex file of MCIMX6S and MXIMX6SX sabred board for config tool?
Please answer.
Thanks.
已解决! 转到解答。
Hi DongHyun
1.2. one can look at ecspi4 configuration and make similar changes for ecspi5
imx6sx-19x19-arm2.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
>3. question. How do I change to slave mode?
please check example on
imx6ul-14x14-evk-ecspi-slave.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, igorpadykov
Thank you for your reply.
In the example in answer 3, remove the spidev0("/delete-node/&spidev0;").
This does not create a spi device in /dev in the slave.
Is there an example of spi device being created in /dev in slave mode?
Thanks.