Using an RT EVK's "freelink" interface to program another RT processor of custom board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using an RT EVK's "freelink" interface to program another RT processor of custom board?

831 Views
solderballz
Contributor I

Can this be done? For example, using the RT1015 EVK, and removing jumpers J45 through J50, then jumping wire from those pins to the respective pins on my custom board -- then using J41 (USB port) to flash from MCUexpresso? I'll probably just power the custom board from another source, while keeping a ground connection between it and the EVK obviously. 

Also, can someone explain what does the "freelink" interface even do and why it's there? I assume to program, but I wanna know more dets

Labels (1)
0 Kudos
Reply
1 Reply

825 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @solderballz ,

  You can remove J44-J50

kerryzhou_0-1654831399975.png

J44-2->customer board POR_B

J47_1->customer board SWD_DIO

J48_1->cusotmer board SWD_CLK

Just make sure the on board RT is removed from the freelink, and connect your own board SWD to the freelink interface.

In fact, I think you also can use our MCU-LINK or MCU-LINK PRO directly to your customer board:

https://www.nxp.com/design/microcontrollers-developer-resources/mcu-link-debug-probe:MCU-LINK

 

https://www.nxp.com/design/microcontrollers-developer-resources/mcu-link-pro-debug-probe:MCU-LINK-PR...

 

Wish it helps you!

Best Regards,

kerry

 

0 Kudos
Reply