Using a generic TFT display with Sabre Lite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using a generic TFT display with Sabre Lite

ソリューションへジャンプ
2,257件の閲覧回数
davidbrooks
Contributor I

Hi all,

I am trying to understand how the parallel LCD display interface is used, from the Sabre Lite schematic.

That board was presumably designed with a particular (class of) display in mind: can someone tell me what it is? Then I'll get it's documentaion, & understand more.

Particularly, I need to understand better what these signals are used for:

PWM1 (pin 37)  - what does this do?

DRDY (pin 34)  - is this Data Enable?

CNTRST (pin 4) - this sounds like "contrast": is it a PWM signal?

Regards & thanks,

ラベル(1)
0 件の賞賛
返信
1 解決策
1,926件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,David,

    I don't konw which schematic you are reading, but normally:

>>PWM1 (pin 37)  - what does this do?

this is PWM signal. there are more 2 PWM modules in i.MX SoC.

>>DRDY (pin 34)  - is this Data Enable?

This is data enable signal.

>>CNTRST (pin 4) - this sounds like "contrast": is it a PWM signal?

Yes, it is PWM signal. used to control back light of LCD.

Regards,

Weidong

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,927件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,David,

    I don't konw which schematic you are reading, but normally:

>>PWM1 (pin 37)  - what does this do?

this is PWM signal. there are more 2 PWM modules in i.MX SoC.

>>DRDY (pin 34)  - is this Data Enable?

This is data enable signal.

>>CNTRST (pin 4) - this sounds like "contrast": is it a PWM signal?

Yes, it is PWM signal. used to control back light of LCD.

Regards,

Weidong

0 件の賞賛
返信
1,926件の閲覧回数
davidbrooks
Contributor I

Many thanks, Weidong.

I was using the Sabre Lite schematic published by Element 14 (aka Farnell Australia), Sheet 15.

Presumably the Sabre was designed with a particular display in mind (connector pinout, etc.) - do you know which that is?

Regards

0 件の賞賛
返信
1,926件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,David,

       Please understand them like above what I described . and would you like to share schematic with me ?

my email : weidong.sun@freescale.com.

     

Thanks,

Weidong

0 件の賞賛
返信