Using a NAND to boot iMX53QSB, and how to enable USBH3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using a NAND to boot iMX53QSB, and how to enable USBH3

1,097 Views
BrunoCostaGarci
Contributor I

Hi,

I have a customer that needs to use the Quickstart board "as is" for a prototype, and wants to use the J13 expansion connector (or any other connector at the board) to connect to a proprietary board, that should have: 1) a NAND flash memory to boot the system; 2) a system to USB Host 3.

However, at the J13 expansion connector, there are no Address lines to use a memory (just data pins, and GPIOs); and the data pins to USBH3 are available, but the control signals (USBH3_nxt, USBH3_DIR, USBH3_CLK e USBH3_STP) are not available.

 

So, this expansion connector is just to connect a Display, or use the serial busses? Is there any way to boot from a NAND flash and use USBH3 at the QSB without making any spider circuit?

Labels (1)
0 Kudos
Reply
0 Replies