Using USB device without VDD5V on imX28

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using USB device without VDD5V on imX28

跳至解决方案
1,452 次查看
MartinHo
Contributor IV

I would like to use the USB OTG Port in device only mode without having VDD5V present. I have seen that there is a patch for Linux L2.6.35_1.1.0 (USB Device not work when VDD5V is not attached during boot (iMX28)).

Is there a similar patch for windows CE 6.0?

best regards

martin

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
1,298 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Martin

I am afraid there are no such patches for WinCE60.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,299 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Martin

I am afraid there are no such patches for WinCE60.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复