Using SWD/JTAG on MIMXRT1011-EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using SWD/JTAG on MIMXRT1011-EVK

1,068 次查看
gfisys
Contributor I

I can't seem to get SWD/JTAG via J-link Ultra to work on the MIMXRT1011-EVK. I've already removed jumpers J61 AND J62, when I initiate debug in MCUExpresso it throws this error message:

2023-04-09 07_44_38-workspace - evkmimxrt1010_igpio_led_output_source_gpio_led_output.c - MCUXpresso.png

Debugging with CMSIS-DAP works fine.

Can you advise? Thanks

标签 (1)
0 项奖励
回复
4 回复数

1,067 次查看
gfisys
Contributor I

Forgot to mention, I connected the J-link to connector J55 on the EVK.

 

 

标记 (1)
0 项奖励
回复

1,048 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @gfisys ,

Have you connect power to EVK?

 

Regards,

Jing

0 项奖励
回复

1,046 次查看
gfisys
Contributor I

Yes, I kept the CMSIS DAP usb connector (J41) plugged in to my PC and the board gets its power from that.

Am I supposed to use an external power supply instead? I didn't see anywhere that being a requirement for using external debugger/programmer.

 

 

0 项奖励
回复

1,034 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @gfisys ,

I tested on my board, it works fine. You can compare the jumper. If nothing different, you can switch the board to serial download mode can check if the MCUBootUtlity can find RT1011. If yes, you can use MCUBootUtlity to erase the flash, then try to connect with jlink again.

jingpan_0-1681197818762.png

 

Regards,

Jing

0 项奖励
回复