Using SSI, I2C, and an external audio codec with Linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using SSI, I2C, and an external audio codec with Linux

1,230 次查看
bobbyeshleman
Contributor I

I'm trying to use an on-board hardware codec with the i.MX6 Solo.  The wm8962 and hardware codec's driver are both configured for I2C.  Should the I2C subsystem be writing to the SSI controller's DMA address instead of the I2C device's address?

I've been referring to application note AN2629 (below), which leads me to believe that directly writing to the I2C device node's address is incorrect.

https://www.nxp.com/docs/en/application-note/AN2628.pdf 

Thanks.

标记 (4)
0 项奖励
回复
1 回复

1,081 次查看
joanxie
NXP TechSupport
NXP TechSupport

pls refer the link as below, hope helpful for you

https://community.nxp.com/thread/432057 

0 项奖励
回复