Hello, I'm running RT1024 on a custom board.
SAI1 is configured as an I2S master to control 1 PCM4104. This DAC is capable of driving 4 output channels, it drives 2 channels per logic state of LRCK:
when LRCK is high, CH1 reproduces whatever comes to DATA0 and CH3 reproduces whatever comes to DATA1.
I'm trying to play sounds taking the "evkmimxrt1024_sai_interrupt_transfer" example and changing SAI3 to SAI1 with the next configuration:
The routine is as follows:
-Initialize clocks
-Initialize SAI1
-Create SAI_TransferTxCreateHandle
STATE_EMITTING_RIGHT
-Turn on LED1
-Configure SAI as left justified, monoright and channel 1 (I leave this channel 1 as the example but don't fully understand why is this value), asynchronous mode, master.
-Configure the SAI_TransferTxSetConfig
-Set the BCK with SAI_TxSetBitClockRate
-Reproduces sound with SAI_TransferSendNonBlocking
-Turn off LED1
STATE_EMITTING_LEFT
-Turn on LED2 and LED3
-Configure SAI as left justified, monoleft and channel 1 (I leave this channel 1 as the example but don't fully understand why is this value), asynchronous mode, master.
-Configure the SAI_TransferTxSetConfig
-Set the BCK with SAI_TxSetBitClockRate
-Reproduces sound with SAI_TransferSendNonBlocking
-Turn off LED2 and LED3
Then repeats alternating playing sound between left and right.
Results:
So far, debugging with MCUxpresso I've been able to reproduce sounds through channel 1 (left) and channel 2 (right).
Issues:
1)This doesn't work all the time, if I try to toggle both LED2 and LED3, the program reproduces 10 times the sound on the left and 9 times on the right and then completely freezes. If I remove writing1&writing0 to LED2 or LED3, the program has no freezing, it alternates reproducing sounds left&right without problem.
1.1) In order to reproduce sounds, I need to run the program through MCUXpresso debugging mode. If I run the program without it, volume goes very low and it only reproduces sound through monoLeft. This doesn't make any sense to me. I'm using the same code I tested on another custom board with the same RT1024 and the same audio DAC, but using SAI3 instead of SAI1
2)I see the audio data coming out from TX_DATA0 but not from TX_DATA1. How could I get data to come out from TX_DATA1 pin too?
I've attached the main programming code files for further detail.
Please, any help would be appreciated!!
Thanks!!
解決済! 解決策の投稿を見る。
I think DEMO_SAI_CHANNEL depend on your needs, what I show you is just a demo.
You can also set saiChannelMask, this param can also set multiple SAI channel.
function -> SAI_TransferTxSetConfig will call SAI_TxSetConfig
In SAI_TxSetConfig function , saiChannelMask set TCR3 register.
BR
mayliu
Hi @DigitalBrain ,
Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.
Question:
1)This doesn't work all the time, if I try to toggle both LED2 and LED3, the program reproduces 10 times the sound on the left and 9 times on the right and then completely freezes. If I remove writing1&writing0 to LED2 or LED3, the program has no freezing, it alternates reproducing sounds left&right without problem.
Answer:
I have download your code, but there are no LED1,LED2,LED3 definition.
when the project freezing, Please check Register, Fault, Peripherals->SAI status.
You can also read SAI status in your code project.
Question:
1.1) In order to reproduce sounds, I need to run the program through MCUXpresso debugging mode. If I run the program without it, volume goes very low and it only reproduces sound through monoLeft. This doesn't make any sense to me. I'm using the same code I tested on another custom board with the same RT1024 and the same audio DAC, but using SAI3 instead of SAI1
Answer:
If the volume changed, I suggest you double check Audio format.
Question:
2)I see the audio data coming out from TX_DATA0 but not from TX_DATA1. How could I get data to come out from TX_DATA1 pin too?
Answer: If you want to use TX_DATA0 and TX_DATA1 of SAI1 , please refer to the content of Section 34.5.1.7 "Transmit Configuration 3 (TCR3)" in the MIMXRT1024RM. You should set the Transmit Enable (TCE) bit in Transmit Configuration 3 (TCR3) when initializing the SAI1.
Wish it helps you.
If you still have question about it, please kindly let me know.
BR
mayliu
Hello @mayliu1
initialization is as follows:
SAI_Init(DEMO_SAI);
SAI_TransferTxCreateHandle(DEMO_SAI, &txHandle, callback, NULL);
SAI_TxSetChannelFIFOMask(DEMO_SAI,3);
I thought that adding the last line would be enough to transmit through TX_DATA1 but it wasn't. What am I missing?
Thanks!!
Hi @DigitalBrain ,
Thanks for your reply.
Could you check your SAI1 TCR3 register value.
You can check MCUXpresso IDE -> Peripherals -> SAI1 -> TCR3->TCE
Wish it helps you.
If you still have question about it, please kindly let me know.
BR
mayliu
Hello, @mayliu1
Thanks for your reply. These are the values:
TCE is set to 0x1.
Maybe I need to use a different function to transmit through TX_DATA1?
Currently I'm using:
sai_handle_t txHandle = {0};
sai_transfer_t xfer;
SAI_TransferSendNonBlocking(SAI1, &txHandle, &xfer);
I understood this function would send the same data at the same time through all the enabled TX_DATA channels. Is it correct?
Thanks!!
Hi, @DigitalBrain
Thanks for your update information.
I notice that your TCE is 1, I don't think it is a right value.
TCE should be 0x03(0b0011) if you want both channel1 and channel 2 working.
Please double check your config function.
BR
mayliu
Hello, @mayliu1
That's true. I've set it to 3:
SAI_TxSetChannelFIFOMask(SAI1,3);
but after executing the function, the register gets set to 0x1 instead of 0x3.
For some reason, I'm not being able to set it to 0x3
Furthermore, even placing the value directly to 0x3 gets 0x1 as result
void SAI_TxSetChannelFIFOMask(I2S_Type *base, uint8_t mask)
{
base->TCR3 &= ~I2S_TCR3_TCE_MASK;
base->TCR3 |= I2S_TCR3_TCE(0x3);
}
Thanks for your update information.
I did a validation on my side, I can set TCE as 0x03, Please refer to what I did.
1: First , I think you should set your SAI TX DATA1 .
Please note that the GPIO TX DATA1 is not real connect, your code should be based on your customed board. The modified configurations I made are just for giving you a demonstration. Please develop your code strictly base on your customed board.
2: Second, you need call SAI_TxSetChannelFIFOMask(DEMO_SAI, 0x03) in your project
I import SDK demo "evkmimxrt1020_sai_interrupt_transfer" , and use MIMXRT1020-EVK board .
Wish it helps you.
If you still have question about it, please kindly let me know.
If you have other question, Please create a new case, Thanks.
BR
mayliu
Hello, @mayliu1
Thanks for your input!
Could you please show me the value you set for DEMO_SAI_CHANNEL?
If I do the following:
#define DEMO_SAI_CHANNEL (0) //Now it doesn't matter as 3 is being hardcoded
SAI_TxSetChannelFIFOMask(DEMO_SAI,5);
SAI_GetLeftJustifiedConfig(&saiConfig, DEMO_AUDIO_BIT_WIDTH, kSAI_MonoRight,3);
The register sets to 3, seems like the value that matters is the sent on SAI_GetLeftJustifiedConfig
Also, how is it possible to select the data to transfer through TX_DATA0 and TX_DATA1 ?
Thanks!
I think DEMO_SAI_CHANNEL depend on your needs, what I show you is just a demo.
You can also set saiChannelMask, this param can also set multiple SAI channel.
function -> SAI_TransferTxSetConfig will call SAI_TxSetConfig
In SAI_TxSetConfig function , saiChannelMask set TCR3 register.
BR
mayliu
Hello @mayliu1
Thanks for your reply!!
Utilizing kSAI_Channel#Mask got me to transmit data through TX_DATA1, however I'm wondering how is it possible to control which data is sent to each of the TX_DATAX.
For example, is it necessary to reconfigure all each time I want to transmit through audio jack1, audiojack2 audiojack3?
Right now, I need to run all of this routine each time I want to transmit through a jack:
Hi @DigitalBrain ,
Thanks for your update information.
Sorry I don't know the corresponding relationship between audio jack1, audiojack2 ,jack3 with your SAI interface.
But I can tell you that SAI_GetClassicI2SConfig, SAI_GetLeftJustifiedConfig, SAI_GetRightJustifiedConfig all can support 2 slot.
Please modify your code, set sai_mono_stereo_t as kSAI_Stereo.
I also suggest you can refer to this link.
https://www.nxp.com/docs/en/application-note/AN12090.pdf
If you still have question, Please create a new case, I will do my best to help you.
BR
mayliu
Thanks @mayliu1 !!
I've checked your previous answer as the solution as now data comes out through TX_DATA1. Also, I'll create a new case to troubleshoot the actual control of the data as suggested
Thanks again!!