Using MIPI_CSI2 1lane mode in i.MX8M EVK

cancel
Showing results for 
Search instead for 
Did you mean: 

Using MIPI_CSI2 1lane mode in i.MX8M EVK

151 Views
larz00
Contributor I

I am trying to use 1 lane mode in i.MX8M EVK.

In the case of imx6, it was supported up to 62.5MHz in 1lane mode.

So, I remember that imx6 can not using HD resolution(74.25MHz) in 1lane mode.

If so, how about maximum bandwidth in imx8m with MIPI_CSI2 1lane mode?

Thanks

Tags (2)
0 Kudos
1 Reply

33 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Daniel

bandwidth is described insect.13.6.1.1 Features i.MX8MDQ Reference Manual:

Supports high speed mode(80Mbps - 1.5Gbps) per lane, providing 4K@30fps
capability for the 4 lanes.

Also sect.13.6.3.4 describes bandwidth capabilities for various data formats.
https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos