Using the MFG Tool to try to EMMC writing.
But this is a kernel panic occurs as follows.
Main chip : I.MX6U
os : Linux
Making the RAMDISK image and to use the MFG Tool, the boot arguments following the u-boot has been passed to the kernel.
2. U-boot boot arguments
3.Kernel command line
Kernel panic occurs when the ramdisk mount, as shown below.
----------------------------------------------------------------------
mxc_dvfs_core_probe
DVFS driver module loaded
regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)
mmc0: new high speed DDR MMC card at address 0001
mmcblk0: mmc0:0001 SEM08G 7.28 GiB
mmcblk0boot0: mmc0:0001 SEM08G partition 1 2.00 MiB
mmcblk0boot1: mmc0:0001 SEM08G partition 2 2.00 MiB
mmcblk0: unknown partition table
mmcblk0boot1: unknown partition table
mmcblk0boot0: unknown partition table
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
[<80045834>] (unwind_backtrace+0x0/0xf8) from [<804bd4d4>] (panic+0x74/0x18c)
[<804bd4d4>] (panic+0x74/0x18c) from [<80008d3c>] (mount_block_root+0x170/0x224)
[<80008d3c>] (mount_block_root+0x170/0x224) from [<80008fc4>] (mount_root+0xe8/0x108)
[<80008fc4>] (mount_root+0xe8/0x108) from [<80009148>] (prepare_namespace+0x164/0x1bc)
[<80009148>] (prepare_namespace+0x164/0x1bc) from [<80008a04>] (kernel_init+0x108/0x13c)
[<80008a04>] (kernel_init+0x108/0x13c) from [<8003faa4>] (kernel_thread_exit+0x0/0x8)
CPU1: stopping
[<80045834>] (unwind_backtrace+0x0/0xf8) from [<80039324>] (do_IPI+0x150/0x17c)
[<80039324>] (do_IPI+0x150/0x17c) from [<8003ea0c>] (__irq_svc+0x4c/0xe8)
Exception stack(0xb8061cf8 to 0xb8061d40)
1ce0: ffffffff b800c7f0
1d00: 8bf9025c ffffffff 80a37b00 b800c7f0 8bf9025c b800c7f0 80a37b00 ffffffff
1d20: 00000000 b8061e34 00000000 b8061d40 80069c60 8022a440 20000113 ffffffff
[<8003ea0c>] (__irq_svc+0x4c/0xe8) from [<8022a440>] (cpumask_next_and+0x14/0x68)
[<8022a440>] (cpumask_next_and+0x14/0x68) from [<80069c60>] (find_busiest_group+0x1ac/0xa30)
[<80069c60>] (find_busiest_group+0x1ac/0xa30) from [<8006a5a4>] (load_balance+0xc0/0x67c)
[<8006a5a4>] (load_balance+0xc0/0x67c) from [<8006ac00>] (rebalance_domains+0xa0/0x18c)
[<8006ac00>] (rebalance_domains+0xa0/0x18c) from [<8006ad30>] (run_rebalance_domains+0x44/0x11c)
[<8006ad30>] (run_rebalance_domains+0x44/0x11c) from [<80075294>] (__do_softirq+0xac/0x140)
[<80075294>] (__do_softirq+0xac/0x140) from [<800757d0>] (irq_exit+0x94/0x9c)
[<800757d0>] (irq_exit+0x94/0x9c) from [<800392e0>] (do_IPI+0x10c/0x17c)
[<800392e0>] (do_IPI+0x10c/0x17c) from [<8003ea0c>] (__irq_svc+0x4c/0xe8)
Exception stack(0xb8061f90 to 0xb8061fd8)
1f80: 80a7b7c0 80000093 00000001 00000000
1fa0: b8060000 80a743e4 804c56b0 80a3b584 1000406a 412fc09a 00000000 00000000
1fc0: 00000000 b8061fd8 8004d708 8003fb04 40000013 ffffffff
[<8003ea0c>] (__irq_svc+0x4c/0xe8) from [<8003fb04>] (default_idle+0x24/0x28)
[<8003fb04>] (default_idle+0x24/0x28) from [<8003fd08>] (cpu_idle+0xc8/0x108)
[<8003fd08>] (cpu_idle+0xc8/0x108) from [<104ba314>] (0x104ba314)
ucl2.xml : mfg tool Settings file
Log.txt : console log file
Original Attachment has been moved to: log.txt.zip
Original Attachment has been moved to: ucl2.xml.zip
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi ryan
had you run DDR tests and rebuild MFG Tools firmware
with new DDR settings found in DDR tests
https://community.freescale.com/docs/DOC-96412
Best regards
igor