Using IPU2 instead of IPU1 of i.MX6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using IPU2 instead of IPU1 of i.MX6Q

991件の閲覧回数
MatthiasWieloch
Contributor I

What changes do I have to make to use IPU2 instead of IPU1.

I'm using a CoM from Karo Electronics (TX6Q) and recompiled the 3.16 Kernel from sources of Karo and my DTS is based on "imx6q-tx6q-10x0.dts.

So far I added a new pinctrl to iomuxc in device tree, use this new pinctrl group for mxcfb0, enabled ipu2 by chaning status from disabled to okay and so far it seems to work. But if I disable IPU1 now the screen stays blank.

Have I missed something

ラベル(3)
0 件の賞賛
返信
1 返信

731件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Matthias

one can look at examples of usage both IPUs

iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信