Lukas,
Do you have a scope? Put it on to J88 SCL pin and try a transaction - you should see square wave about 92 KHz. If it's there, there's likely something wrong with your device. If not, I2C bus is not getting initialized properly. Are you using /dev/i2c-0 to access I2C? It's available in LTIB kernel configuration.
If you see the SCL pulses but still no luck, I recommend spending a couple hundred dollars on a I2C bus analyzer. It will read what's flying on SCL and SDA. Here are two options:
http://www.zeroplus.com.tw/logic-analyzer_en/products.php?pdn=1&product_id=250
(inexpensive, works)
http://www.totalphase.com/products/beagle_ism/
(a bit more expensive, better software)
Hi Lukas...
About the LTIB package Im not familiar with that, maybe somebody of software can help you to bring up that i2c.
-ni
Hi
You do not need to add the eeprom (24LCxx-I/P) if you are going to use it, you can add or make you connection from here (J88) to your chip,
something that I forget, do not add pull up resistor because the board already have them for SCL & SDA.
-ni
Hi Lucas.
Maybe SAMTEC directly can help you with a sample but if not, the no populated dip socket with reference J88 pins 6 I2C0_SCL & pin 5 I2C0_SDA you can make the connections.
regards
-ni
Hi Lukas,
If you need the I2C to connect externally to other board in the J78 (LCD PORT) of the EVK, pins 31 for SCL and pin 29 for SDA if this is in use you can move to the J63 pin 109 & 107, respectively. Those net are connected to the default state of the pad, this means after reset you will have i2c communication by default.
hope this can help you.
-ni