Using HAB on an iMX6 Nitrogen board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using HAB on an iMX6 Nitrogen board

1,891 次查看
jamesdemers
Contributor I

I'm trying to use the HAB to sign, and eventually encrypt & decrypt, a U-Boot image on a Nitrogen board.  I've followed the instructions I've found so far, and I've created a U-Boot image from the U-Boot repository at git://github.com/boundarydevices/u-boot-imx6.git, using the production branch.

I've signed the image using the cst tool (ver 2.3.1), and I've examined the byte-codes in the resulting image, and everything looks good to me.  I programmed the SPI flash on the board, and it boots U-Boot properly, but the hab_status command results in

U-Boot > hab_status

Secure boot disabled

HAB Configuration: 0xf0, HAB State: 0x66

--------- HAB Event 1 -----------------

event data:

        0xdb 0x00 0x14 0x41 0x33 0x06 0xc0 0x00

        0xbe 0x00 0x0c 0x00 0x09 0x17 0x00 0x02

        0x00 0x00 0x11 0x00

--------- HAB Event 2 -----------------

event data:

        0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00

        0x00 0x00 0x00 0x00 0x17 0x7f 0xf4 0x00

        0x00 0x00 0x00 0x20

--------- HAB Event 3 -----------------

event data:

        0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00

        0x00 0x00 0x00 0x00 0x17 0x7f 0xf4 0x2c

        0x00 0x00 0x03 0x18

--------- HAB Event 4 -----------------

event data:

        0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00

        0x00 0x00 0x00 0x00 0x17 0x7f 0xf4 0x20

        0x00 0x00 0x00 0x01

--------- HAB Event 5 -----------------

event data:

        0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00

        0x00 0x00 0x00 0x00 0x17 0x80 0x00 0x00

        0x00 0x00 0x00 0x04

U-Boot >

Now those seem to be problems (HAB_INV_COMMAND and HAB_INV_ASSERTIONs), and I'm stuck as to how to proceed.  I've replicated the same issue using the main-line U-Boot distro and the Freescale one, so I'm sure it's something I'm doing or not doing.  I can provide more detail on any portion of this, but I was hoping for some advice on how to proceed before I start burning fuses and such.

标签 (2)
0 项奖励
回复
1 回复

1,535 次查看
michaelrobbelot
Contributor IV

James,

You seem to be experiencing some of the same issues that I am. You can take a look at https://community.freescale.com/message/524573#524573  and my commits on https://github.com/PDi-Communication-Systems-Inc/u-boot_v2009.08/commits/ar6mx_hab  to see if that helps you out.

If you figure out anything, please let me know.

Michael Robbeloth

0 项奖励
回复