Using GPT1 in Linux on iMX8MPlus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using GPT1 in Linux on iMX8MPlus

跳至解决方案
1,480 次查看
alexeyfirago
Contributor II

Hi all,

We have a custom board based on iMX8MPlus. We want to use GPT1 to capture a signal on SAI3_TXC. We are using kernel revision imx-5.4.47_2.2.0 and revision imx-atf imx_5.4.47_2.2.0.

Is it possible to use GPT1 in Linux? Will adding a DTS node for GPT be enough? Or we also should patch imx8mp_bl31_setup.c in imx-atf?

Thanks!

标签 (1)
0 项奖励
回复
1 解答
1,475 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alexey

 

patch was sent via mail.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,476 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alexey

 

patch was sent via mail.

 

Best regards
igor

0 项奖励
回复