We have a custom board with a IMX6UL. The IMX is connected to a generic PHY using RMII.
ENET1_TX_CLK is configured as ENET1_REF_CLK1, and should be an output from the PHY at 25MHz (I think).
ENET2_RX_EN is configured as ENET1_REF_CLK_25M and should be an output from the IMX to the PHY at 25MHz.
I'm using u-boot ATM, and have the following code:
static iomux_v3_cfg_t const fec1_pads[] = {
...MX6_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 | MUX_PAD_CTRL(ENET_CLK_PAD_CTRL),
MX6_PAD_ENET2_RX_EN__ENET1_REF_CLK_25M | MUX_PAD_CTRL(ENET_CLK_PAD_CTRL),
...
};int board_eth_init(bd_t *bis)
{
imx_iomux_v3_setup_multiple_pads(fec1_pads, ARRAY_SIZE(fec1_pads));...
}
static int setup_fec(void)
{
struct iomuxc *const iomuxc_regs = (struct iomuxc *)IOMUXC_BASE_ADDR;
int ret;// Use ENET1_TX_CLK as an input
// Set GRP1[13] - ENET1_CLK_SEL - get ENET1 Tx clk from ENET1_TX_CLK pin
// clear GPR1[17] - ENET1_TX_CLK_DIR - output driver is disabled
clrsetbits_le32(&iomuxc_regs->gpr[1], IOMUX_GPR1_FEC1_MASK,
IOMUX_GPR1_FEC1_CLOCK_MUX2_SEL_MASK);ret = enable_fec_anatop_clock(0, ENET_25MHZ);
if (ret)
{
printf("Failed to enable clock\n");
return ret;
}enable_enet_clk(1);
return 0;
}
Unfortunately there appears to be nothing outputted on the REF_CLK_25M signal.
I can't see much in the TRM on how to enable this. As far as I can tell just muxing the ENET2_RX_EN as ENET1_REF_CLK_25M should be enough. There's no reference to clock gating or anything else that I can find.
Any ideas?
Thanks,
Andrew
解決済! 解決策の投稿を見る。
Hi Igor,
I had the muxing set OK.
The problem was the BM_ANADIG_PLL_ENET_REF_25M_ENABLE bit in the pll_enet register.
Andrew
Hi Andrew
for muxing ENET2_RX_EN as ENET1_REF_CLK_25M one can use
register IOMUXC_SW_MUX_CTL_PAD_ENET2_RX_EN described in
sect.30.5.55 SW_MUX_CTL_PAD_ENET2_RX_EN SW MUX Control
Register (IOMUXC_SW_MUX_CTL_PAD_ENET2_RX_EN) i.MX6UL Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
I had the muxing set OK.
The problem was the BM_ANADIG_PLL_ENET_REF_25M_ENABLE bit in the pll_enet register.
Andrew