Using EMMC v4.5 or higher as boot device with imx.6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using EMMC v4.5 or higher as boot device with imx.6

1,228 次查看
emilzachariageo
Contributor II

Hi

The imx.6 datasheet says about emmc support upto v4.41.

I wanted to use emmc as boot device. As v4.41 or earlier devices are less available these days, can I use the available v4.5 or higher devices?

I read from another community feed that it is't possible.

I'm giving this question to confirm.

Thanks.

0 项奖励
回复
1 回复

894 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Emil

yes it is possible, boot ROM will fall back to the eMMC4.41 standard

when a eMMC4.5 capable device is detected. For usage in linux

one can look at

i.mx6 with eMMC 5.0 SDR or DDR interface?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复