As per the imx7 secure boot design, Booting is happening using the root of trust. Is there any way that without using verification I can boot up the board? i.e. Just for the POC, i want to run the "secure boot" SDK/software without verification, I will not be using the signed image.So verification is also not required. Is it possible to do that?
@jiteshka
Hello,
i.MX7 board can be booted even if a boot image cannot pass verification
correctly - when the i.MX7 is not (secure) closed. But it is not possible to run
unsigned boot image - by boot ROM - if the i.MX7 is closed.
If the boot image is correctly signed - it can load and run any image.
Regards,
Yuri.
By default (fuse configuration of) i.MX7 is in non secure (open) mode.
Yes - If the boot image is not signed and i.MX7 is not closed (i.e. non-secure mode)
then the boot-ROM allows the boot image to run.
~Yuri.