Use of OnSemi AR0820 instead of AR0821 on iMX8MP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use of OnSemi AR0820 instead of AR0821 on iMX8MP?

2,305 Views
hns80
Senior Contributor I

Since the AR0820 and AR0821 are very similar, could the AR0820 be used with the iMX8MP with the existing AR0821 driver?

0 Kudos
Reply
2 Replies

1,807 Views
LilianeD
Contributor II

Hello,

Where is the driver for AR821? is it basler-camera-driver-vvcam?

Regards,

0 Kudos
Reply

2,296 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello hns80,

The MX8MP has the driver for AR821, the AR820 has change the connection in MIPI, it can communicate but the driver in the BSP correspond to AR821, you have to adapt the driver.

 

Regards

 

0 Kudos
Reply