Use cst tool to verify signature of images

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Use cst tool to verify signature of images

3,085 次查看
haGkiu
Contributor I

Hello community,

 

I want to use cst tool to sign binary images of my software and then use the same tool to verify the signed software( verify that they are signed correctly)

Is that possible with cst tool ?

Can anyone help me .

 

 

 

0 项奖励
回复
7 回复数

3,050 次查看
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @haGkiu ,

I hope you're doing well!

Can you let me know what processor are you using? And is it an EVK or a custom board?

Thank you.

Best regards,
Hector.

0 项奖励
回复

3,013 次查看
haGkiu
Contributor I

Hello,

I am using a phytec phycore card with an imx6q processor.

 

0 项奖励
回复

3,006 次查看
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @haGkiu ,

In order to verify/authenticate a signed image you can use the U-Boot command hab_auth_img

3.4 Verifying HAB events
-------------------------

The U-Boot includes the hab_auth_img command which can be used for
authenticating and troubleshooting the signed image, zImage must be
loaded at the load address specified in the IVT.

- Authenticate additional image:

=> hab_auth_img <Load Address> <Image Size> <IVT Offset>

If no HAB events were found the zImage is successfully signed.

I'd recommend the following guide for secure boot in i.MX 6 devices: uboot-imx/doc/imx/habv4/guides/mx6_mx7_secure_boot.txt at lf_v2022.04 · nxp-imx/uboot-imx · GitHub

Let me know if this was of any help.

Best regards,
Hector.

0 项奖励
回复

2,998 次查看
haGkiu
Contributor I

Hello,

 

I am working with barebox not u_boot , do you have any information on how to sign barebox with cst (so it can be authenticated by hab).

0 项奖励
回复

2,961 次查看
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @haGkiu ,

Other bootloaders besides our U-Boot are currently out of our scope of support, so we don't have any previous tests/guides/examples using barebox for our CST software. Our tools were also designed around our software in this case, but I won't be able to confirm 100% if the process would be the same or if some critical modifications would be needed to ensure barebox compatibility. Is there a particular reason to not use U-boot?

Best regards,
Hector.

0 项奖励
回复

2,901 次查看
haGkiu
Contributor I

Hello @hector_delgado ,

The company in which I work is using barebox as a boatloder on the project.

Do you have an idea if there is a tool I can use to sign barebox ( to be authenticated by HAB module on imx6 electronic cards).

Best regards,

Moufida.

 

 

0 项奖励
回复

2,890 次查看
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @haGkiu ,

From previous cases I've found the following link to barebox documentation which apparently has built in support for CST: https://www.barebox.org/doc/latest/boards/imx.html#high-assurance-boot

I can't guarantee full compatibility but I think it's worth to look at.

Thank you.

Best regards,
Hector.

0 项奖励
回复