Use UUU to load flash.bin with M4 Image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use UUU to load flash.bin with M4 Image

2,989 Views
jmcdowell
Contributor II

Hello,

My intention is to boot just the Cortex-M4 (not the A-35s) of the iMX8QX from eMMC

I have generated a flash.bin using the imx-mkimage target: flash_cm4. Specifically, in order to generate flash.bin, I ran "make SOC=iMX8QX flash_cm4".

I then attempted to use the latest version of uuu (1.4.72) in order to download the image into eMMC.  I am including my invocation and failure output below.

  • Is "uuu -b emmc flash.bin" the proper invocation of uuu in order to download an m4-only flash.bin into the eMMC?
  • Does the failure output below indicate anything useful in regards to something I might have done wrong in obtaining the SCFW SECOFW?

 

sudo /home/jmcdowell/bin/uuu -b emmc flash.bin           
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.72-0-g8e9e189

Success 0    Failure 0                                                                                         
                                                                                                               
                                                                                                               
1:1      1/ 0 [                                      ]                                                          
Success 0    Failure 0                                                                                         
                                                                                                               
                                                                                                               
1:1      1/ 1 [                                      ] SDPS: boot -f flash.bin                                  
Success 0    Failure 0                                                                                         
                                                                                                               
                                                                                                               
1:1      1/ 1 [====>            13%                  ] SDPS: boot -f flash.bin                                  
Success 0    Failure 0                                                                                         
                                                                                                               
                                                                                                               
1:1      1/ 1 [=========>       27%                  ] SDPS: boot -f flash.bin                                  
Success 0    Failure 0                                                                                         
                                                                                                               
                                                                                                               
1:1      1/ 1 [==============>  41%                  ] SDPS: boot -f flash.bin                                  
Success 0    Failure 0                                                                                         
                                                                                                               
                                                                                                               
1:1      1/ 1 [=================55%>                 ] SDPS: boot -f flash.bin                                  
Success 0    Failure 0                                                                                         
                                                                                                               
                                                                                                               
1:1      1/ 1 [=================69%=====>            ] SDPS: boot -f flash.bin                                  
Success 0    Failure 0                                                                                         
                                                                                                               
                                                                                                               
1:1      1/ 1 [=================83%==========>       ] SDPS: boot -f flash.bin                                  
Success 0    Failure 1                                                                                         
                                                                                                               
                                                                                                               
1:1      1/ 1 [HID(W):LIBUSB_ERROR_IO                ] SDPS: boot -f flash.bin                                  
Success 0    Failure 1                                                                                         
                                                                                                               
                                                                                                               
1:1      1/ 1 [HID(W):LIBUSB_ERROR_IO                ] SDPS: boot -f flash.bin

0 Kudos
Reply
2 Replies

2,977 Views
BiyongSUN
NXP Employee
NXP Employee

because you need the u-boot and u-boot fast boot running for flashing the emmc. 

and the image flash.bin you built only has the m4. that is why flash gets fail. 

 

if you look at the uuu help. 

you will see  arg0: _flash.bin bootloader and  arg1: _image[Optional] image burn to emmc, default is the same as bootloader. it is optional.

So for you case, you need two arg0 and arg1. arg0 is the bootloader flash.bin has u-boot and arg1 is what you want to burn to emmc. 

So you can use the binary release to burn the flash.bin you built. 

uuu -b emmc imx-boot-imx8qxpc0mek-sd.bin-flash  flash.bin

here imx-boot-imx8qxpc0mek-sd.bin-flash is the flash.bin with u-boot(running on A35 and has uboot fastboot). flash.bin here is you build with "make SOC=iMX8QX flash_cm4".

 

uuu [-d -m -v] -b[run] <emmc|emmc_all|fat_write|nand|qspi|sd|sd_all|spl> arg...
Run Built-in scripts
emmc burn boot loader to eMMC boot partition
arg0: _flash.bin bootloader
arg1: _image[Optional] image burn to emmc, default is the same as bootloader
emmc_all burn whole image to eMMC
arg0: _flash.bin
arg1: _rootfs.sdcard
fat_write update one file in fat partition, require uboot fastboot running in board

0 Kudos
Reply

2,958 Views
jmcdowell
Contributor II

Thank you for your quick response and for providing this clarification.  I can not use the binary release since I am not using the evaluation kit but rather another System-on-Module.  But I now understand that my path forward is to build u-boot for my platform with fastboot configured.  I then need to generate the appropriate flash.bin using the this custom u-boot and arm trusted firmware for my board (make SOC=iMX8QX flash).  Then I should be set up to use 'uuu' properly providing both arguments.

 

Justin

0 Kudos
Reply