Use Torizon Core Builder to build imx6ull image for SoM with raw NAND

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Use Torizon Core Builder to build imx6ull image for SoM with raw NAND

1,332 次查看
vgelinski
Contributor I

Hi,

I am pretty new to Torizon OS. I have SoM board that has raw NAND memory. I want to build custom image for it using the Torizon Core Builder. In the Input section I am passing this URL as remote source: "https://artifacts.toradex.com/artifactory/torizoncore-oe-prod-frankfurt/kirkstone-6.x.y/release/8/co.... Note that this is image for eMMC, not for raw NAND. So, as expected I get error while trying to install thie generated image with Toradex Easy Installer. When I connect to the VNC server at 192.168.11.1, I get the following error: Error message
I am getting the download link from this list . But I don't see image for imx6ull board with raw NAND memory. My question is, how do I get a link to the correct image, or how should I modify the tcbuild.yaml config file, so that I get the correct output.


P.s. I have a sample config file for buildroot, and it works. But now I want to try Torizon Core Builder. I can compare the two image.json file - one generated by Buildroot, and one generated by using Torizon Core Builder. So, I know in general how to modify the image.json file, but I don't want to do it manually. In the best case scenario, I should modify only tcbuild.yaml file, and it should generate correct image.json file.

0 项奖励
回复
2 回复数

1,330 次查看
vgelinski
Contributor I

Sorry, image not attached in original post. Here is the error message:
https://ibb.co/d6cJC4F

0 项奖励
回复

1,321 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Maybe someone from @Torizon will help.

Regards

0 项奖励
回复