Use Mouse on i.MX6 SABRE AI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use Mouse on i.MX6 SABRE AI

934 Views
florianl
Contributor III

Hi everybody,

I would like to use an optical mouse on the  i.MX6 SABRE AI. At the moment I'm using the YOCTO build fsl-image-gui from the dylan branch.

I already have the provided usb cable mini->normal attached but the mouse is never activated...

Thanks alot!

Florian

Labels (3)
0 Kudos
Reply
2 Replies

626 Views
LeonardoSandova
Specialist I

Is there any log on dmesg's output (kernel log) when you connect it? Does it work on your Linux Host?

Leo

0 Kudos
Reply

626 Views
florianl
Contributor III

Hi Leo,

thanks for your quick reply.

No the dmesg doesn't show any output when connecting the mouse. On the host the mouse is working flawlessly Also the otpical mouse light doesn't turn on...

correction/addition to my previous post: I'm using the J10 USB-OTG connector on the CPU board with the provided usb-cable (Micro-B to standard-A cable and A-female to A-female adaptor)

The only usb related outputs in dmesg:

usbcore: registered new interface driver usbfs                            
usbcore: registered new interface driver hub                              
usbcore: registered new device driver usb                                 
IMX usb wakeup probe                                                      
IMX usb wakeup probe                                                      
usbcore: registered new interface driver usb-storage                      
usbcore: registered new interface driver btusb                            
usbcore: registered new interface driver usbhid                           
usbhid: USB HID core driver                                               

usbcore: registered new interface driver snd-usb-audio

0 Kudos
Reply