Use JTAG debugger imx8qxp colibri with an M4 application in DDR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Use JTAG debugger imx8qxp colibri with an M4 application in DDR

1,884 次查看
gmterhorst
Contributor II

Hi,

We have a working debugger setup in Windows with SEGGER Ozone when the M4_0 application is linked for TCM memory.
We can also successfully run a TCM or a DDR application when the M4_0 is started from U-Boot. The one thing we cannot do is upload a DDR application via SEGGER Ozone (or any other JTAG debugger/flasher for that matter).

Is it possible to do such a thing, or can DDR applications only be loaded via the SCU/U-Boot? And if it is possible: how?

Kind regards,

Thijs

5 回复数

1,837 次查看
gmterhorst
Contributor II

Hi Dhruvit,

Thank you for your answer. Unfortunately it is not the answer I am looking for. As I tried to explain in the first line, we can successfully run an example with JTAG from Windows when compiling for TCM. We can also successfully run a TCM or a DDR application when the M4_0 is started from U-Boot. The one thing we cannot do is upload a DDR application via JTAG.

Is it possible to do such a thing, or can DDR applications only be loaded via the SCU/U-Boot? And if it is possible: how?

Kind regards,

Thijs

0 项奖励
回复

1,787 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @gmterhorst,

I hope you are doing well

The one thing we cannot do is upload a DDR application via JTAG.
=> Please confirm the term "DDR application" is the binary for the M4 core or not.
Kindly mention where you are trying to upload the application i.e. MMC or DDR etc.
 
Thanks & Regards,
Dhruvit Vasavada
0 项奖励
回复

1,755 次查看
gmterhorst
Contributor II

Hi @Dhruvit 

I am indeed talking about the binary for the M4_0 core in the imx8qxp, which we link to run from DDR (similar to what the "build_ddr_release.sh"/"build_ddr_debug.sh" scripts in all the SDK examples armgcc directories do).

Kind regards,

Thijs

0 项奖励
回复

1,689 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @gmterhorst,

I hope you are doing well.

Yes, Before loading the application, the DDR should be initialized properly that's why the DDR application can be loaded via SCU/Uboot. Direct loading of the application without Uboot is not possible.
 

Thanks & Regards,
Dhruvit Vasavada

0 项奖励
回复

1,849 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @gmterhorst,

I hope you are doing well
 
To run the application using JTAG, kindly refer to section 5.1.3 Run an example application(Linux host) and section 5.2.3 Run an example application(windows host) from the document Getting Started with MCUXpresso SDK for i.MX 8QuadXPlus
 
Thanks & Regards,
Dhruvit Vasavada
0 项奖励
回复