Use Chromium will crashing unexpectedly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use Chromium will crashing unexpectedly

1,689 Views
felixhsu
Contributor III

Hi All

I had testing result as below.

Platform: i.MX6Q-SDB
OS: Linux 4.1.5_2.1.0
APP: Chromium 48.0.2548.0

1. Use Ethernet cable on board then boot Linux and click Chromium icon will crashing unexpectedly (fail rate 100%).
2. Boot Linux and click chromium icon is normal, then connect Ethernet cable is normal, but create new tab will crashing unexpectedly (fail rate 100%).
3. Boot Linux and click chromium icon is normal, don’t use Ethernet cable connect on the board, chromium always is normal.

How to fixed this problem.

Thanks.

Labels (4)
0 Kudos
Reply
2 Replies

1,517 Views
JayTu
NXP Employee
NXP Employee

Asking FAE (jim.lin) to move it to internal then we can monitor it. Will update it after getting progress later.

0 Kudos
Reply

1,517 Views
JayTu
NXP Employee
NXP Employee

I'll check it after back to office. 

0 Kudos
Reply