Updating the M-Core image without the bootloader (iMX8ULP)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Updating the M-Core image without the bootloader (iMX8ULP)

917件の閲覧回数
dhruvinrajpura
Contributor III

Hi,
I want to update the M-core image without modifying the bootloader. Typically, the flash.bin file contains components such as the AHAB container, UPower firmware, U-Boot, and the M-core binary. However, I only want to update the M-core image, not the bootloader or other components.

Is it possible to do this?

If yes how can I make that image and how can I flash it?


Thanks,
RDS

 

タグ(4)
0 件の賞賛
返信
3 返答(返信)

780件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi 

Please have a reference from the Chapter 4 of This guide there are guides related to M core images

 

Regards

Harvey

0 件の賞賛
返信

768件の閲覧回数
dhruvinrajpura
Contributor III

Hi Harvey,
I have already gone through that reference manual, but unfortunately, it does not contain the section for i.MX8ULP (section 4.7.4).

I did find some community posts mentioning that on i.MX93, we can use remoteproc to update the M-core image from the A-core. I’m wondering if someone has already patched this functionality into the i.MX8ULP, and whether we can use it now?

Here are links for those posts:
https://community.nxp.com/t5/i-MX-Processors/i-MX8ULP-remoteproc-error-and-how-to-run-different-bina...
https://community.nxp.com/t5/i-MX-Processors/How-to-update-the-M33-firmware-using-remoteproc-on-iMX8...

0 件の賞賛
返信

605件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

As you can see the support from the update-the-M33-firmware-using-remoteproc-on-iMX8ULP 

With checking internal team, so far, no definitive reply for our BSP.

 

Regards

Harvey

0 件の賞賛
返信