Hi,
I want to update the M-core image without modifying the bootloader. Typically, the flash.bin file contains components such as the AHAB container, UPower firmware, U-Boot, and the M-core binary. However, I only want to update the M-core image, not the bootloader or other components.
Is it possible to do this?
If yes how can I make that image and how can I flash it?
Thanks,
RDS
Hi
Please have a reference from the Chapter 4 of This guide there are guides related to M core images
Regards
Harvey
Hi Harvey,
I have already gone through that reference manual, but unfortunately, it does not contain the section for i.MX8ULP (section 4.7.4).
I did find some community posts mentioning that on i.MX93, we can use remoteproc to update the M-core image from the A-core. I’m wondering if someone has already patched this functionality into the i.MX8ULP, and whether we can use it now?
Here are links for those posts:
https://community.nxp.com/t5/i-MX-Processors/i-MX8ULP-remoteproc-error-and-how-to-run-different-bina...
https://community.nxp.com/t5/i-MX-Processors/How-to-update-the-M33-firmware-using-remoteproc-on-iMX8...
As you can see the support from the update-the-M33-firmware-using-remoteproc-on-iMX8ULP
With checking internal team, so far, no definitive reply for our BSP.
Regards
Harvey