Updated Default Display Orientation for Android 10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Updated Default Display Orientation for Android 10

2,174件の閲覧回数
tpe
Contributor III

Hello,

My aim is to change the default display orientation to portrait mode on a iMX8M device running the AndroidQ-10.0.0 release. I found an older thread that referenced a couple patches that allows the property ro.sf.hwrotation to be configured for my needs here. However, these patches no longer hold for Android 10. Are there any updates patches? If not, is there another updated way to achieve this?

Thank you,

Tony 

0 件の賞賛
返信
3 返答(返信)

2,133件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello tpe,

 

The latest BSP for android 10 is https://www.nxp.com/webapp/Download?colCode=Q10.0.0_2.3.0_ANDROID_SOURCE&appType=license

 

That includes the patch for display rotation, however you can add buildin SF_PRIMARY_DISPLAY_ORIENTATION=90  or  "content insert " cmd control at run time.

Regards

 

0 件の賞賛
返信

1,575件の閲覧回数
edward_fu
Contributor III

Hi Bio,

I have the same problem. I added SF_PRIMARY_DISPLAY_ORIENTATION=90 in BoardConfig.mk. But it seems no use. I did as this thread How-to-make-android-system-display-vertically-rotate-270-degree

0 件の賞賛
返信

2,061件の閲覧回数
tpe
Contributor III

Hello,

 

Thank you for your help! How do I rotate the touch input as well? Also, is there another property for secondary/multi-displays? Something like SF_SECONDARY_DISPLAY_ORIENTATION? 

 

Best regards,
Tony

0 件の賞賛
返信