Hi
In our custom board design with i.MX8DualXPlus / i.MX8QuadXPlus, based on the MEK, we do not require the Ethernet functionality. The hardware developer guide does not mention about the i.MX8 QXP unused input/output guidance for ethernet signal IO's.
Can we leave them unconnected as shown below:
Please advise.
Regards
Solved! Go to Solution.
Hello,
According to i.MX8 QM/i.MX8 QXP Hardware Developer’s Guide, the following takes place for
Ethernet pins: digital I/O supplies can be left unconnected when the associated I/O balls are
not in use (left floating).
CAUTION:
Driving/connecting associated I/O balls is prohibited when the supply isn’t powered.
Also, the Ethernet pins can be configured as GPIO, in such case the supply voltages must be applied.
Regards,
Yuri.
Hello,
According to i.MX8 QM/i.MX8 QXP Hardware Developer’s Guide, the following takes place for
Ethernet pins: digital I/O supplies can be left unconnected when the associated I/O balls are
not in use (left floating).
CAUTION:
Driving/connecting associated I/O balls is prohibited when the supply isn’t powered.
Also, the Ethernet pins can be configured as GPIO, in such case the supply voltages must be applied.
Regards,
Yuri.