I have already fixed the problem.
I mixed up with the location of the file updater_ivt.sb which was originally I thought placed in ./litb/rootfs/boot. In fact it is stored in the same location as ./ltib.
Eric
Hi guys,
I am trying to create the updater_ivt.sb used by Mfgtools for my board as well but failed to do so.
I have followed the steps shown below but still not able to create the updater_ivt.sb file
2.5 Building the Manufacturing Firmware (To Be Supported)
Refer to Section 2.2 Installing and Building LTIB, to setup the ltib environment.
Configure the firmware build profile
$ ./ltib --selectype
Choose the following:
--- Choose the platform type
Selection (imx28) --->
--- Choose the packages profile
Selection (mfg firmware profile) --->
Save and exit.
After ltib completes the build, Updater.sb and updater_ivt.sb will have been created.
If you are able to create it, please help by providing any hints or guidance.
Eric