Unmatch about DDR DDR Output Driver Average Impedance for i.MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unmatch about DDR DDR Output Driver Average Impedance for i.MX53

Jump to solution
1,106 Views
ko-hey
Senior Contributor II

Hi all

 

I have questions about DDR calibration resistance in Output Driver Average Impedance for i.MX53.

 

As it mentioned in following thread, the Table 43-2 and 43.3.454 unmatched and we have same question.

But there didn't answer the thread.

https://community.nxp.com/thread/328744

 

Q1.

Table 43-2 does not describe the DSE value when it set DDR3 dde_sel = 01.

Refer to 43.3.454 IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE and it is explained as "NVCC_EMI_DRAM = 1.5 V +/- 5% (DDR 3), ddr_sel = '' 01: 160 Ohm '

 

In the case of dde_sel = 01 setting of DDR3, is the value of DSE the same as DDR_SEL = 01/11 of LPDDR 2 mode in Table 43-2 ?

 

Q2.

If Q1 is not same, could you provide a DSE value when it set DDR3 dde_sel = 01 ?

 

Q3.

We think that the calibration resistance which is shows in yellow line is wrong.

Because there are no settings in Table 43.3.454.

 

The correct calibration resistance is 200 Ohm. Am I correct ?

 

231892_231892.jpgimage002.jpg

 

 

Ko-hey

Labels (5)
0 Kudos
1 Solution
852 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

>Q1.2

please refer to below description

pastedImage_1.jpg

>Q3

correct is 240 Ohm

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
853 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

>Q1.2

please refer to below description

pastedImage_1.jpg

>Q3

correct is 240 Ohm

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
852 Views
TomE
Specialist II

The table you quote lists resistances of 240, 120, 80, 60, 48, 48 and 34.

In the thread quoted from the original post in this thread, I pointed out the above values are wrong and gave corrections. That was back in August 2014. I had to look in the i.MX6 manual to get the correct values (which are 48 and 40).

i.MX53 Reference Manual Errors, is there a list? 

I would suggest the original poster do the same. When in doubt, read a newer manual for a different product.

In the above thread, four years ago, gusarambula reported these bugs, but said it might take "some time" for these to be fixed. He also said these postings are likely to be the only places you'll see these sort of corrections.

Tom

0 Kudos