Unexpected deassertion occurs in WEIM in i.MX253

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unexpected deassertion occurs in WEIM in i.MX253

Jump to solution
733 Views
ko-hey
Senior Contributor II

Hi all

 

I have question about ENGcm11891 which is described in IMX25CE Rev. 7.1.

 

 

Q1.

Does the timing of OE deassertion synchronize with the address switching ?

 

What I care about is that if / OE is deasserted at the timing of latching data, ROM can not output data,

so I think that it affects the data to be acquired, but when we confirmed by oscilloscope, address change timing It seems that / OE is deasserting.

At this timing, since it is different from the timing of latching data, we think that it can be designed so that there is no problem.

 

Q2.

Does the CE deassert in synchronization with the change of the address signal at the completion of the burst access ?

 

 

Ko-hey

 

Labels (2)
0 Kudos
Reply
1 Solution
560 Views
art
NXP Employee
NXP Employee

1. The effect of the erratum is so that some glitches occur on the OE#, EB# and LBA# signals during the address switch in the page emulation mode. The shape of these glitches is unpredictable. The OE# glitch can affect the data setup time so that wrong data may be latched. So, better is to follow the recommended workaround.

2. The CE# signal is not affected by the erratum. It is deasserted synchronously with the address deassertion at the end of the access.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
561 Views
art
NXP Employee
NXP Employee

1. The effect of the erratum is so that some glitches occur on the OE#, EB# and LBA# signals during the address switch in the page emulation mode. The shape of these glitches is unpredictable. The OE# glitch can affect the data setup time so that wrong data may be latched. So, better is to follow the recommended workaround.

2. The CE# signal is not affected by the erratum. It is deasserted synchronously with the address deassertion at the end of the access.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply