PMIC MMPF0100F0ZES
We have VCOREDIG connected to VDDOTP through a 100k resistor for the default configuration, from which we expect to see 2.5 V on VGEN5 per MMPF0100Z Rev 9.0, 12/2015
However, when we power up we see ~3.1 V on this rail.
Is it possible that something in the HW design is causing this issue?
Is the datasheet incorrect?
Hello,
1.
The recent PMIC Datasheet may be found at
2.
You are right, for default configuration for VGEN5 (VCOREDIG connected to VDDOTP through 100k),
it should provide 2.5 V. Please check the design regarding PMIC erratum ER19.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Yuri,
1) Thanks for the datasheet link.
2) I don't think this error applies. The regulators that I expect to start up all do. The issue is overvoltage on one of the regulators. However, I have tried connecting LICELL to our main 3.3 V supply (it is the first supply up on the board, and also feeds the PMIC) to bypass this issue--the change had no effect on VGEN5's output voltage.
3) I have found something else: the VCOREDIG and VDDOTP pins are at 2.7 V instead of the expected 1.5 V. The only component connected to these pins is the 100k resistor joining them.
Regards,
Nick
Hello,
Let me look at the scheme (the PMIC and all its power consumers).
You may create request for it : How to submit a new question for NXP Support
Also, please provide PMIC photo with its part number.
Regards,
Yuri.