Hi,
We are trying to record and playback audio from MCIMX6Q-SDB board using ALSA but its not working.
We have connected an external mic to the audio jack.
While studying the schematic to understand the issue we came across a particular input to the audio module called CODEC_PWR_EN. Is it a problem with the processor not switching on this GPIO?
Attached is the screenshot of the schematic mentioning CODEC_PWR_EN.
Please let us know if someone had faced issues using mic on this board? If so can you please help us get the mic working?
Thanks and regards,
Shreesha
Hello,
Please use Chapter 28 [Advanced Linux Sound Architecture (ALSA) System on
a Chip (ASoC) Sound Driver] of the recent Linux BSP for some details about
audio support implementation. In particular, please refer to section 28.5 (Unit Test)
Also the following may be useful :
Audio recording is not working on BSP v3.14.28
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------