Unable to play short duration WMA files during HTTP progressive download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to play short duration WMA files during HTTP progressive download

941 Views
mghasan
Contributor I

Hi,

 

WMA audio playback with short duration (1-15 secs) is not working with streaming of HTTP progressive download in custom board based on IMX6.

 

Set up:

1. You need HTTP progressive download URL with .wma file and with duration less than 1 - 15 seconds.

ex: http://xx.xx.xx.xxx/download/voicemail32678.wav?key=1H3zasefKJbEevWWsiAoIzycLBVuWH

2. Open URL from application and play

 

And we are getting below error and please find complete attached logs.

 

01-13 06:18:28.510: I/OMXPlayer(32124): Connecting http://xx.xx.xx.xx/download/voicemail30.wav?key=Fs80RMMEHFblf8FNusEIBPZdtcRu3s

01-13 06:18:28.510: I/OMXPlayer(32124): GET /download/voicemail30.wav?key=Fs80RMMEHFblf8FNusEIBPZdtcRu3s HTTP/1.1

01-13 06:18:28.510: I/OMXPlayer(32124): User-Agent: Android;Linux;iPad;iPhone

01-13 06:18:28.510: I/OMXPlayer(32124): Accept: */*

01-13 06:18:28.510: I/OMXPlayer(32124): Host: 10.99.88.52

01-13 06:18:28.510: I/OMXPlayer(32124): ffurl_write 165

01-13 06:18:28.510: I/OMXPlayer(32124): retry_transfer_wrapper size 165 size_min 165

01-13 06:18:28.510: I/OMXPlayer(32124): retry_transfer_wrapper: calling transfer_func

01-13 06:18:28.510: I/OMXPlayer(32124): retry_transfer_wrapper: called transfer_func, ret = 165

01-13 06:18:28.510: I/OMXPlayer(32124): retry_transfer_wrapper OUT with len 165

01-13 06:18:28.510: I/OMXPlayer(32124): ffurl_read 2048

01-13 06:18:28.510: I/OMXPlayer(32124): retry_transfer_wrapper size 2048 size_min 1

01-13 06:18:28.510: I/OMXPlayer(32124): retry_transfer_wrapper: calling transfer_func

01-13 06:18:28.610: I/OMXPlayer(32124): retry_transfer_wrapper: called transfer_func, ret = -11

 

url_read() functions is taking 3 seconds to get the http response in non working case and in working case url_read() immediately returns.

 

If we disable Freescale GM_Player from Stagefright and mediaplayerservice .mk fiels and play with NuPlayer, it works fine.

Original Attachment has been moved to: omxplayer-error-log.txt.zip

0 Kudos
2 Replies

505 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community. 

0 Kudos

505 Views
mghasan
Contributor I

Thanks Wlodek_D. Moved to i.MX Community.

0 Kudos