Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0"

ソリューションへジャンプ
5,459件の閲覧回数
ThanarajS
Contributor III

U-Boot 2014.04-08637-gaffa032 (May 11 2016 - 10:04:29)

 

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

CPU:   Temperature 37 C, calibration data: 0x5ab4f27d

Reset cause: WDOG

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

Found PFUZE100 deviceid=10,revid=11

check_and_clean: reg 0, flag_set 0

Fastboot: Normal

flash target is MMC:2

Net:   FEC [PRIME]

Normal Boot

Hit any key to stop autoboot:  0

booti mmc2

kernel   @ 14008000 (6723120)

ramdisk  @ 15000000 (497370)

fdt      @ 14f00000 (50782)

kernel cmdline:

        use boot.img command line:

        console=ttymxc0,115200 androidboot.console=ttymxc0 consoleblank=0 vmalloc=256M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 vidM

switch to ldo_bypass mode!

   Using Device Tree in place at 14f00000, end 14f0f65d

 

Starting kernel ...

 

Booting Linux on physical CPU 0x0

Initializing cgroup subsys cpu

Initializing cgroup subsys cpuacct

Linux version 3.10.53-06481-g1c3a910 (b18293@scmbld4) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #4 SMP PREEMPT Thu Jan 8 14:16:27 5

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 Quad SABRE Smart Device Board

cma: CMA: reserved 384 MiB at 32000000

Memory policy: ECC disabled, Data cache writealloc

PERCPU: Embedded 8 pages/cpu @817d9000 s9728 r8192 d14848 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 259840

Kernel command line: console=ttymxc0,115200 androidboot.console=ttymxc0 consoleblank=0 vmalloc=256M init=/init video=mxcfb0:dev=hdmi,1920x1080M@M

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 959MB 64MB = 1023MB total

Memory: 627668k/627668k available, 420908k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0xc0800000 - 0xff000000   (1000 MB)

    lowmem  : 0x80000000 - 0xc0000000   (1024 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .text : 0x80008000 - 0x80e51868   (14631 kB)

      .init : 0x80e52000 - 0x80ea7600   ( 342 kB)

      .data : 0x80ea8000 - 0x80f2b740   ( 526 kB)

       .bss : 0x80f2b740 - 0x80fc02f8   ( 595 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Preemptible hierarchical RCU implementation.

NR_IRQS:16 nr_irqs:16 16

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

CPU identified as i.MX6Q, silicon rev 1.2

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Security Framework initialized

SELinux:  Initializing.

Mount-cache hash table entries: 512

Initializing cgroup subsys debug

Initializing cgroup subsys freezer

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x807bf708 - 0x807bf760

CPU1: Booted secondary processor

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

CPU2: Booted secondary processor

CPU2: thread -1, cpu 2, socket 0, mpidr 80000002

CPU3: Booted secondary processor

CPU3: thread -1, cpu 3, socket 0, mpidr 80000003

Brought up 4 CPUs

SMP: Total of 4 processors activated (6324.22 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

pinctrl core: initialized pinctrl subsystem

regulator-dummy: no parameters

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

Use WDOG2 as reset source

syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered

vdd1p1: 800 <--> 1375 mV at 1125 mV

vdd3p0: 2800 <--> 3150 mV at 3000 mV

vdd2p5: 2000 <--> 2750 mV at 2425 mV

cpu: 725 <--> 1450 mV

vddpu: 725 <--> 1450 mV

vddsoc: 725 <--> 1450 mV

syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered

syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered

!!request miniPCIE Power On gpio

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

bio: create slab <bio-0> at 0

mxs-dma 110000.dma-apbh: initialized

usb_otg_vbus: 5000 mV

usb_h1_vbus: 5000 mV

wm8962-supply: no parameters

mipi_dsi_pwr_on: no parameters

sensor-supply: 3300 mV

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c i2c-0: IMX I2C adapter registered

i2c i2c-1: IMX I2C adapter registered

i2c i2c-2: IMX I2C adapter registered

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed

mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Initialized.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

pureg-dummy: no parameters

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 4, 65536 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

TCP: reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

Freeing initrd memory: 484K (85000000 - 85079000)

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

imx6_busfreq busfreq.16: DDR medium rate not supported.

Bus freq driver module loaded

bt power gpio is:2

mxc_bt_rfkill driver success loaded

rfkill: BT RF going to : on

mxc_bt_rfkill_reset

mxc_ir consumer_ir.41: unable to request PWM.

platform consumer_ir.41: Driver mxc_ir requests probe deferral

console [pstore-1] enabled

ramoops: attached 0x100000@0x4bf00000, ecc: 0/0

mxc_ramoops device success loaded

futex hash table entries: 1024 (order: 4, 65536 bytes)

audit: initializing netlink socket (disabled)

type=2000 audit(0.480:1): initialized

VFS: Disk quotas dquot_6.5.2

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

NTFS driver 2.1.30 [Flags: R/W DEBUG].

jffs2: version 2.2. (NAND) �용 2001-2006 Red Hat, Inc.

fuse init (API version 7.22)

msgmni has been set to 1994

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

imx-weim 21b8000.weim: WEIM driver registered.

mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed

MIPI DSI driver module loaded

imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_DISP0_DAT9 already requested by 2084000.pwm; cannot claim for lcd.34

imx6q-pinctrl 20e0000.iomuxc: pin-101 (lcd.34) status -22

imx6q-pinctrl 20e0000.iomuxc: could not request pin 101 on device 20e0000.iomuxc

mxc_lcdif lcd.34: Error applying setting, reverse things back

imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_DISP0_DAT9 already requested by 2084000.pwm; cannot claim for lcd.34

imx6q-pinctrl 20e0000.iomuxc: pin-101 (lcd.34) status -22

imx6q-pinctrl 20e0000.iomuxc: could not request pin 101 on device 20e0000.iomuxc

mxc_lcdif lcd.34: Error applying setting, reverse things back

mxc_lcdif lcd.34: can't get/select pinctrl

mxc_lcdif: probe of lcd.34 failed with error -22

mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1

fbcvt: 1920x1080@60: CVT Name - 2.073M9

mxc_sdc_fb fb.30: registered mxc display driver hdmi

imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

Console: switching to colour frame buffer device 240x67

mxc_sdc_fb fb.31: Can't get fb option for mxcfb1!

mxc_sdc_fb fb.32: Can't get fb option for mxcfb2!

mxc_sdc_fb fb.33: Can't get fb option for mxcfb3!

imx-sdma 20ec000.sdma: no iram assigned, using external mem

imx-sdma 20ec000.sdma: loaded firmware 1.1

imx-sdma 20ec000.sdma: initialized

pfuze100-regulator 1-0008: Full lay: 1, Metal lay: 1

pfuze100-regulator 1-0008: FAB: 0, FIN: 0

pfuze100-regulator 1-0008: pfuze100 found.

SW1AB: 300 <--> 1875 mV at 1150 mV

SW1C: 300 <--> 1875 mV at 1175 mV

SW2: 800 <--> 3300 mV at 3300 mV

SW3A: 400 <--> 1975 mV at 1500 mV

SW3B: 400 <--> 1975 mV at 1500 mV

SW4: 800 <--> 3300 mV at 3150 mV

SWBST: 5000 <--> 5150 mV at 5000 mV

VSNVS: 1000 <--> 3000 mV at 3000 mV

VREFDDR: 750 mV

VGEN1: 800 <--> 1550 mV at 1500 mV

VGEN2: 800 <--> 1550 mV at 1500 mV

VGEN3: 1800 <--> 3300 mV at 2800 mV

VGEN4: 1800 <--> 3300 mV at 1800 mV

VGEN5: 1800 <--> 3300 mV at 3000 mV

VGEN6: 1800 <--> 3300 mV at 3300 mV

Serial: IMX driver

2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

console [ttymxc0] enabled

21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX

21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 62) is a IMX

serial: Freescale lpuart driver

imx sema4 driver is registered.

[drm] Initialized drm 1.1.0 20060810

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop: module loaded

imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_KEY_COL1 already requested by 21f4000.serial; cannot claim for 2008000.ecspi

imx6q-pinctrl 20e0000.iomuxc: pin-128 (2008000.ecspi) status -22

imx6q-pinctrl 20e0000.iomuxc: could not request pin 128 on device 20e0000.iomuxc

spi_imx 2008000.ecspi: Error applying setting, reverse things back

m25p80 spi32766.0: found mr25h256, expected m25p32

m25p80 spi32766.0: mr25h256 (32 Kbytes)

spi_imx 2008000.ecspi: probed

tun: Universal TUN/TAP device driver, 1.6

tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>

CAN device driver interface

libphy: fec_enet_mii_bus: probed

fec 2188000.ethernet eth0: registered PHC device 0

PPP generic driver version 2.4.2

PPP BSD Compression module registered

PPP Deflate Compression module registered

PPP MPPE Compression module registered

NET: Registered protocol family 24

usbcore: registered new interface driver asix

usbcore: registered new interface driver ax88179_178a

usbcore: registered new interface driver cdc_ether

usbcore: registered new interface driver net1080

usbcore: registered new interface driver cdc_subset

usbcore: registered new interface driver zaurus

usbcore: registered new interface driver cdc_ncm

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

usbcore: registered new interface driver cdc_acm

cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters

usbcore: registered new interface driver usb-storage

usbcore: registered new interface driver usbserial

usbcore: registered new interface driver option

usbserial: USB Serial support registered for GSM modem (1-port)

ci_hdrc ci_hdrc.0: EHCI Host Controller

ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00

usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb1: Product: EHCI Host Controller

usb usb1: Manufacturer: Linux 3.10.53-06481-g1c3a910 ehci_hcd

usb usb1: SerialNumber: ci_hdrc.0

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

ci_hdrc ci_hdrc.1: doesn't support gadget

ci_hdrc ci_hdrc.1: EHCI Host Controller

ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2

usb 1-1: new high-speed USB device number 2 using ci_hdrc

ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

usb usb2: New USB device found, idVendor=1d6b, idProduct=0002

usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb2: Product: EHCI Host Controller

usb usb2: Manufacturer: Linux 3.10.53-06481-g1c3a910 ehci_hcd

usb usb2: SerialNumber: ci_hdrc.1

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

mousedev: PS/2 mouse device common for all mice

usbcore: registered new interface driver xpad

usbcore: registered new interface driver usb_acecad

usbcore: registered new interface driver aiptek

usbcore: registered new interface driver gtco

usbcore: registered new interface driver hanwang

usbcore: registered new interface driver kbtab

usbcore: registered new interface driver wacom

usb 1-1: New USB device found, idVendor=05e3, idProduct=0608

usb 1-1: New USB device strings: Mfr=0, Product=1, SerialNumber=0

usb 1-1: Product: USB2.0 Hub

hub 1-1:1.0: USB hub found

hub 1-1:1.0: 4 ports detected

elan-touch 2-0010: elan - Read Hello Packet Failed

elan-touch: probe of 2-0010 failed with error -22

egalax_ts 1-0004: Failed to read firmware version

egalax_ts: probe of 1-0004 failed with error -5

egalax_ts 2-0004: Failed to read firmware version

egalax_ts: probe of 2-0004 failed with error -5

input: max11801_ts as /devices/soc0/soc.1/2100000.aips-bus/21a4000.i2c/i2c-1/1-0048/input/input0

i2c-core: driver [isl29023] using legacy suspend method

i2c-core: driver [isl29023] using legacy resume method

snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0

i2c /dev entries driver

ov5640_read_reg:write reg error:reg=300a

camera ov5640 is not found

usb 1-1.1: new low-speed USB device number 3 using ci_hdrc

ov5642_read_reg:write reg error:reg=300a

camera ov5642 is not found

usb 1-1.1: New USB device found, idVendor=0461, idProduct=4e22

usb 1-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=0

usb 1-1.1: Product: USB Optical Mouse

usb 1-1.1: Manufacturer: PixArt

ov5640_read_reg:write reg error:reg=300a

camera ov5640_mipi is not found

mxc_v4l2_output v4l2_out.38: V4L2 device registered as video16

mxc_v4l2_output v4l2_out.38: V4L2 device registered as video17

usbcore: registered new interface driver uvcvideo

USB Video Class driver (1.1.1)

gspca_main: v2.14.0 registered

usb 1-1.3: new high-speed USB device number 4 using ci_hdrc

mag3110 2-000e: check mag3110 chip ID

input: FreescaleMagnetometer as /devices/virtual/input/input1

input: eCompass as /devices/virtual/input/input2

mag3110 2-000e: mag3110 is probed

usb 1-1.3: New USB device found, idVendor=1618, idProduct=9113

usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=6

usb 1-1.3: Product: Wireless USB Network Module

usb 1-1.3: Manufacturer: Redpine Signals, Inc.

usb 1-1.3: SerialNumber: 000000000001

input: FreescaleAccelerometer as /devices/virtual/input/input3

mma8x5x device driver probe successfully

imx2-wdt 20c0000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)

usb 1-1.4: new low-speed USB device number 5 using ci_hdrc

device-mapper: uevent: version 1.0.3

device-mapper: ioctl: 4.24.0-ioctl (2013-01-15) initialised: dm-devel@redhat.com

Bluetooth: Virtual HCI driver ver 1.3

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCIATH3K protocol initialized

usbcore: registered new interface driver btusb

cpuidle: using governor ladder

cpuidle: using governor menu

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

mmc1: no vqmmc regulator found

mmc1: no vmmc regulator found

mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA

mmc2: no vqmmc regulator found

mmc2: no vmmc regulator found

usb 1-1.4: New USB device found, idVendor=413c, idProduct=2107

usb 1-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber=0

usb 1-1.4: Product: Dell USB Entry Keyboard

usb 1-1.4: Manufacturer: DELL

mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA

mmc3: no vqmmc regulator found

mmc3: no vmmc regulator found

mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA

Galcore version 5.0.11.25762

mmc2: new high speed SDHC card at address e624

mmcblk2: mmc2:e624 SU08G 7.40 GiB

mmcblk2: p1 p2 p3 < p5 p6 p7 p8 > p4

mmcblk2: p4 size 13352010 extends beyond EOD, truncated

mmc3: new high speed DDR MMC card at address 0001

mmcblk3: mmc3:0001 SEM08G 7.39 GiB

mmcblk3boot0: mmc3:0001 SEM08G partition 1 1.00 MiB

mmcblk3boot1: mmc3:0001 SEM08G partition 2 1.00 MiB

mmcblk3rpmb: mmc3:0001 SEM08G partition 3 128 KiB

mmcblk3: p1 p2 p3 < p5 p6 p7 p8 p9 > p4

mmcblk3: p4 size 13303808 extends beyond EOD, truncated

mmcblk3boot1: unknown partition table

mmcblk3boot0: unknown partition table

mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

mxc_asrc 2034000.asrc: mxc_asrc registered

mxc_vpu 2040000.vpu: VPU initialized

hidraw: raw HID events driver (C) Jiri Kosina

input: PixArt USB Optical Mouse as /devices/soc0/soc.1/2100000.aips-bus/2184000.usb/ci_hdrc.0/usb1/1-1/1-1.1/1-1.1:1.0/input/input4

hid-generic 0003:0461:4E22.0001: input,hidraw0: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-ci_hdrc.0-1.1/input0

input: DELL Dell USB Entry Keyboard as /devices/soc0/soc.1/2100000.aips-bus/2184000.usb/ci_hdrc.0/usb1/1-1/1-1.4/1-1.4:1.0/input/input5

hid-generic 0003:413C:2107.0002: input,hidraw1: USB HID v1.11 Keyboard [DELL Dell USB Entry Keyboard] on usb-ci_hdrc.0-1.4/input0

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

ashmem: initialized

logger: created 256K log 'log_main'

logger: created 256K log 'log_events'

logger: created 256K log 'log_radio'

logger: created 256K log 'log_system'

usbcore: registered new interface driver snd-usb-audio

wm8962 0-001a: customer id 0 revision D

input: WM8962 Beep Generator as /devices/soc0/soc.1/2100000.aips-bus/21a0000.i2c/i2c-0/0-001a/input/input6

imx-wm8962 sound.28:  wm8962 <-> 202c000.ssi mapping ok

imx-audio-hdmi sound-hdmi.29:  hdmi-hifi <-> hdmi_audio.17 mapping ok

NET: Registered protocol family 26

u32 classifier

    Actions configured

Netfilter messages via NETLINK v0.30.

nf_conntrack version 0.5.0 (15958 buckets, 63832 max)

ctnetlink v0.93: registering with nfnetlink.

NF_TPROXY: Transparent proxy support initialized, version 4.1.0

NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.

xt_time: kernel timezone is -0000

ip_tables: (C) 2000-2006 Netfilter Core Team

arp_tables: (C) 2002 David S. Miller

TCP: cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 10

mip6: Mobile IPv6

ip6_tables: (C) 2000-2006 Netfilter Core Team

NET: Registered protocol family 17

NET: Registered protocol family 15

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

can: raw protocol (rev 20120528)

can: broadcast manager protocol (rev 20120528 t)

can: netlink gateway (rev 20130117) max_hops=1

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: BNEP socket layer initialized

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

Bluetooth: HIDP socket layer initialized

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

VGEN1: disabling

SWBST: disabling

SW4: disabling

wm8962-supply: disabling

regulator-dummy: disabling

imx mcc test is registered.

file system registered

android_usb gadget: Mass Storage Function, version: 2009/09/11

android_usb gadget: Number of LUNs=1

lun0: LUN: removable file: (no medium)

android_usb gadget: android_usb ready

input: gpio-keys.27 as /devices/soc0/gpio-keys.27/input/input7

snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)

ALSA device list:

  #0: wm8962-audio

  #1: imx-hdmi-soc

Freeing unused kernel memory: 340K (80e52000 - 80ea7000)

SELinux:  Permission attach_queue in class tun_socket not defined in policy.

SELinux: the above unknown classes and permissions will be denied

type=1403 audit(1.750:2): policy loaded auid=4294967295 ses=4294967295

SELinux: Loaded policy from /sepolicy

type=1404 audit(1.760:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295

init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.

init: /dev/hw_random not found

keychord: using input dev DELL Dell USB Entry Keyboard for fevent

keychord: using input dev gpio-keys.27 for fevent

init: cannot open '/initlogo.rle'

Console: switching to colour dummy device 80x30

EXT4-fs (mmcblk2p5): mounted filesystem with ordered data mode. Opts: (null)

EXT4-fs (mmcblk2p4): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk2p4): warning: maximal mount count reached, running e2fsck is recommended

EXT4-fs (mmcblk2p4): recovery complete

EXT4-fs (mmcblk2p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic

EXT4-fs (mmcblk2p6): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk2p6): warning: maximal mount count reached, running e2fsck is recommended

EXT4-fs (mmcblk2p6): recovery complete

EXT4-fs (mmcblk2p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit

EXT4-fs (mmcblk2p7): mounted filesystem with ordered data mode. Opts: (null)

init: /dev/hw_random not found

rfkill: BT RF going to : off

type=1400 audit��IةT�Q]�T�_�]���M�n�healthd: BatteryTemperaturePath not found

init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'

healthd: BatteryTechnologyPath not found

init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead

init: property 'ro.serialno' doesn't exist while expanding '$ro.serialno'

init: cannot expand '$ro.serialno' while writing to '/sys/class/android_usb/android0/iSerial'

init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead

init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead

init: property 'sys.powerctl' doesn't exist while expanding '${sys.powerctl}'

init: powerctl: cannot expand '${sys.powerctl}'

init: property 'sys.sysctl.extra_free_kbytes' doesn't exist while expanding '${sys.sysctl.extra_free_kbytes}'

init: cannot expand '${sys.sysctl.extra_free_kbytes}' while writing to '/proc/sys/vm/extra_free_kbytes'

android_usb: already disabled

mtp_bind_config

binder: 153:153 transaction failed 29189, size 0-0

root@sabresd_6dq:/ # ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

warning: `zygote' uses 32-bit capabilities (legacy support in use)

period 1975891114 ,timeout is -66172562, wake up is :0

period 1975891114 ,timeout is -66172562, wake up is :0

request_suspend_state: wakeup (3->0) at 22682548668 (1970-01-02 00:00:04.484456000 UTC)

period 66 ,timeout is 0, wake up is :0

mma enable setting active

lowmemorykiller: lowmem_shrink: convert oom_adj to oom_score_adj:

lowmemorykiller: oom_adj 0 => oom_score_adj 0

lowmemorykiller: oom_adj 1 => oom_score_adj 58

lowmemorykiller: oom_adj 2 => oom_score_adj 117

lowmemorykiller: oom_adj 3 => oom_score_adj 176

lowmemorykiller: oom_adj 9 => oom_score_adj 529

lowmemorykiller: oom_adj 15 => oom_score_adj 1000

fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)

IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready

acc_open

acc_release

onebox_wlan_nongpl: module license 'unspecified' taints kernel.

Disabling lock debugging due to kernel taint

usbcore: registered new interface driver Onebox-USB

init: sys_prop: permission denied uid:1003  name:service.bootanim.exit

libphy: 2188000.ethernet:01 - Link is Up - 100/Full

IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

Unable to register the devicewlan0

ERROR: Failed to create vap_interface

VAP = NULL

request_suspend_state: sleep (0->3) at 37991512670 (2016-05-19 08:58:00.152605667 UTC)

active wake lock PowerManagerService.Broadcasts

active wake lock PowerManagerService.WakeLocks

mma enable setting inactive

 

root@sabresd_6dq:/ # busyUnable to register the devicewlan0

ERROR: Failed to create vap_interface

VAP = NULL

root@sabresd_6dq:/ # netcfg                                                   

rpine0   DOWN                                   0.0.0.0/0   0x00001802 00:23:a7:5c:53:10

wlan0    DOWN                                   0.0.0.0/0   0x00001002 00:23:a7:5c:53:10

eth0     UP                               192.168.3.107/24  0x00001043 00:04:9f:03:cd:f9

lo       UP                                   127.0.0.1/8   0x00000049 00:00:00:00:00:00

root@sabresd_6dq:/ # logcat | grep Wifi

I/AudioFlinger(  163): loadHwModule() Loaded r_submix audio interface from Wifi Display audio HAL (audio) handle 4

D/WifiMonitor(  462): Creating WifiMonitor

D/WifiMonitor(  462): WifiMonitorSingleton gotten

D/WifiMonitor(  462): WifiMonitorSingleton created

D/WifiMonitor(  462): registerInterface(p2p0+android.net.wifi.p2p.WifiP2pService$P2pStateMachine@2ca00990)

E/WifiStateMachine(  462): RPS WiFi state machine starting with interface name as wlan0andwlan0

D/WifiMonitor(  462): Creating WifiMonitor

D/WifiMonitor(  462): WifiMonitorSingleton gotten

D/WifiMonitor(  462): registerInterface(wlan0+android.net.wifi.WifiStateMachine@2ca0ffa0)

D/WifiStateMachine(  462): completeConstruction: E

D/WifiStateMachine(  462): completeConstruction: maxDepth=6

D/WifiStateMachine(  462): setupInitialStateStack: E mInitialState=InitialState

D/WifiStateMachine(  462): moveTempStackToStateStack: i=1,j=0

D/WifiStateMachine(  462): moveTempStackToStateStack: i=0,j=1

D/WifiStateMachine(  462): moveTempStackToStateStack: X mStateStackTop=1,startingIndex=0,Top=InitialState

D/WifiStateMachine(  462): completeConstruction: X

D/WifiStateMachine(  462): handleMessage: E msg.what=-2

D/WifiStateMachine(  462): invokeEnterMethods: DefaultState

D/WifiStateMachine(  462): invokeEnterMethods: InitialState

D/WifiController(  462): isAirplaneModeOn = false, isWifiEnabled = true, isScanningAvailable = false

E/WifiHW  (  462): Mutyam**** Disabling protocol

E/WifiHW  (  462):

I/WifiService(  462): WifiService starting up with Wi-Fi enabled

D/WifiService(  462): setWifiEnabled: true pid=462, uid=1000

D/WifiController(  462): WifiController msg { when=0 what=155656 target=com.android.internal.util.StateMachine$SmHandler } deferred for 213ms

D/WifiController(  462): DEFERRED_TOGGLE handled

D/WifiStateMachine(  462): setting operational mode to 1

E/WifiApConfigStore(  462): Bad version on hotspot configuration file, set defaults

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131154

D/WifiStateMachine(  462): processMsg: InitialState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131084

D/WifiStateMachine(  462): processMsg: InitialState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131085

D/WifiStateMachine(  462): processMsg: InitialState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131146

D/WifiStateMachine(  462): processMsg: InitialState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131083

D/WifiStateMachine(  462): processMsg: InitialState

E/WifiHW  (  462): Loading WiFi driver here

E/WifiHW  (  462): *****common_gpl.ko inserted

E/WifiHW  (  462): *****wlan.ko inserted

E/WifiHW  (  462): ****wlan_wep.ko inserted

E/WifiHW  (  462): *****wlan_tkip.ko inserted

E/WifiHW  (  462): *****wlan_ccmp.ko inserted

E/WifiHW  (  462): ********wlan_acl.ko inserted

E/WifiHW  (  462): *****wlan_xauth.ko inserted

E/WifiHW  (  462): ***wlan_scan_sta.ko inserted

E/WifiHW  (  462): ***onebox_wlan_nongpl.ko inserted

E/WifiHW  (  462): ***onebox_wlan_gpl.ko inserted

E/WifiHW  (  462): ***onebox_bt_nongpl.ko inserted

E/WifiHW  (  462): ***onebox_bt_gpl.ko inserted

E/WifiHW  (  462): *****onebox_nongpl.ko inserted

E/WifiHW  (  462): ***********onebox_gpl.ko

E/WifiHW  (  462): ********* ALL ko inserted successfully

E/WifiHW  (  157): Mutyam****protocol enable

E/WifiHW  (  157):

E/WifiHW  (  157): RAVI:****Vap Creation Output:

E/WifiHW  (  157):

E/WifiHW  (  157): RAVI:****Inside STA wifi.c wifi_get_fw_path out_iface is wlan0

E/WifiHW  (  157): Mutyam****protocol enable

E/WifiHW  (  157):

E/WifiHW  (  157): RAVI:****Vap Creation Output:

E/WifiHW  (  157):

E/WifiHW  (  157): RAVI:****Inside AP wifi.c wifi_get_fw_path out_iface is wlan0

D/WifiMonitor(  462): WifiMonitorSingleton gotten

D/WifiStateMachine(  462): setWifiState: enabling

D/WifiStateMachine(  462): Supplicant start successful

D/WifiMonitor(  462): WifiMonitorSingleton gotten

D/WifiMonitor(  462): startMonitoring(wlan0) with mConnected = false

D/WifiMonitor(  462): connecting to supplicant

E/WifiHW  (  462): Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0": Permission denied

E/WifiHW  (  462): Supplicant not running, cannot connect

E/WifiHW  (  462): Supplicant not running, cannot connect

E/WifiHW  (  462): Supplicant not running, cannot connect

E/WifiHW  (  462): Supplicant not running, cannot connect

E/WifiHW  (  462): Supplicant not running, cannot connect

E/WifiMonitor(  462): startMonitoring(wlan0) failed!

D/WifiStateMachine(  462): transitionTo: destState=SupplicantStartingState

D/WifiStateMachine(  462): handleMessage: new destination call exit/enter

D/WifiStateMachine(  462): setupTempStateStackWithStatesToEnter: X mTempStateStackCount=1,curStateInfo: state=DefaultState,active=true,parent=nul

D/WifiStateMachine(  462): invokeExitMethods: InitialState

D/WifiStateMachine(  462): moveTempStackToStateStack: i=0,j=1

D/WifiStateMachine(  462): moveTempStackToStateStack: X mStateStackTop=1,startingIndex=1,Top=SupplicantStartingState

D/WifiStateMachine(  462): invokeEnterMethods: SupplicantStartingState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131144

D/WifiStateMachine(  462): processMsg: SupplicantStartingState

D/WifiStateMachine(  462): deferMessage: msg=131144

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131085

D/WifiStateMachine(  462): processMsg: SupplicantStartingState

D/WifiStateMachine(  462): deferMessage: msg=131085

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131149

D/WifiStateMachine(  462): processMsg: SupplicantStartingState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): setSuspendOptimizations: 2 true

D/WifiStateMachine(  462): mSuspendOptNeedsDisabled 0

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=69632

D/WifiStateMachine(  462): processMsg: SupplicantStartingState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131101

D/WifiStateMachine(  462): processMsg: SupplicantStartingState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131101

D/WifiStateMachine(  462): processMsg: SupplicantStartingState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131206

D/WifiStateMachine(  462): processMsg: SupplicantStartingState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=147458

D/WifiStateMachine(  462): processMsg: SupplicantStartingState

E/WifiStateMachine(  462): Failed to setup control channel, restart supplicant

D/WifiMonitor(  462): WifiMonitorSingleton gotten

D/WifiStateMachine(  462): transitionTo: destState=InitialState

D/WifiStateMachine(  462): handleMessage: new destination call exit/enter

D/WifiStateMachine(  462): setupTempStateStackWithStatesToEnter: X mTempStateStackCount=1,curStateInfo: state=DefaultState,active=true,parent=nul

D/WifiStateMachine(  462): invokeExitMethods: SupplicantStartingState

D/WifiStateMachine(  462): moveTempStackToStateStack: i=0,j=1

D/WifiStateMachine(  462): moveTempStackToStateStack: X mStateStackTop=1,startingIndex=1,Top=InitialState

D/WifiStateMachine(  462): invokeEnterMethods: InitialState

E/WifiHW  (  462): Mutyam**** Disabling protocol

E/WifiHW  (  462):

D/WifiStateMachine(  462): moveDeferredMessageAtFrontOfQueue; what=131085

D/WifiStateMachine(  462): moveDeferredMessageAtFrontOfQueue; what=131144

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131144

D/WifiStateMachine(  462): processMsg: InitialState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131085

D/WifiStateMachine(  462): processMsg: InitialState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleScreenStateChanged: true

D/WifiStateMachine(  462): handleMessage: E msg.what=131154

D/WifiStateMachine(  462): processMsg: InitialState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131127

D/WifiStateMachine(  462): processMsg: InitialState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131158

D/WifiStateMachine(  462): processMsg: InitialState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): setSuspendOptimizations: 4 false

D/WifiStateMachine(  462): mSuspendOptNeedsDisabled 4

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleScreenStateChanged: false

D/WifiStateMachine(  462): handleMessage: E msg.what=131154

D/WifiStateMachine(  462): processMsg: InitialState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131158

D/WifiStateMachine(  462): processMsg: InitialState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): setSuspendOptimizations: 4 true

D/WifiStateMachine(  462): mSuspendOptNeedsDisabled 0

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131083

D/WifiStateMachine(  462): processMsg: InitialState

E/WifiHW  (  157): Mutyam****protocol enable

E/WifiHW  (  157):

E/WifiHW  (  157): RAVI:****Vap Creation Output:

E/WifiHW  (  157):

E/WifiHW  (  157): RAVI:****Inside STA wifi.c wifi_get_fw_path out_iface is wlan0

E/WifiHW  (  157): Mutyam****protocol enable

E/WifiHW  (  157):

E/WifiHW  (  157): RAVI:****Vap Creation Output:

E/WifiHW  (  157):

E/WifiHW  (  157): RAVI:****Inside AP wifi.c wifi_get_fw_path out_iface is wlan0

D/WifiMonitor(  462): WifiMonitorSingleton gotten

E/WifiStateMachine(  462): Failed to start supplicant!

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131101

D/WifiStateMachine(  462): processMsg: InitialState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

D/WifiStateMachine(  462): handleMessage: E msg.what=131101

D/WifiStateMachine(  462): processMsg: InitialState

D/WifiStateMachine(  462): processMsg: DefaultState

D/WifiStateMachine(  462): handleMessage: X

^C

130|root@sabresd_6dq:/ # logcat | grep wpa_                                   

E/WifiHW  (  462): Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0": Permission denied

I/wpa_supplicant(  914): Successfully initialized wpa_supplicant

E/wpa_supplicant(  914): wlan0: Unsupported driver 'nl80211'

I/wpa_supplicant( 1051): Successfully initialized wpa_supplicant

E/wpa_supplicant( 1051): wlan0: Unsupported driver 'nl80211'

 

Here i am facing issue with unable to open connection to supplicant on /data/system/wpa_supplicant/wlan0.Actually there is no wlan0 file in this /data/system/wpa_supplicant/ directory.

 

Que1:

How it ( "wlan0" ) will create in /data/syatem/wpa_supplicant/ directory ? For this problem i have changed all possible permissions in init.rc file.

By default wlan0 will create or we have to create ?..if we have create means,.please tell me the steps to do???

 

If wlan0 is created in /data/system/wpa_supplicant/,we establish connection to supplicant.So this error i need to fix first.

 

Que2:

And For Unsupported driver "nl80211", i compiled wpa_supplicant using bsd interface but its taking nl80211 ?..

i have enabled CONFIG_DRIVER_BSD=y in all files(defconfig,android.config,wpa_cli.c,...etc).Eventhough i am getting Unsupported driver error.

 

Last two weeks i am facing this problem.please anyone give solution for this issue.

 

Any Solutions.......!!!!

Original Attachment has been moved to: logs.zip

Regards,
Thanaraj Subramani
ラベル(1)
0 件の賞賛
返信
1 解決策
3,411件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Raj,

    Refer to the link, please!

Porting BCM4330/BCM43362 WIFI to Android4.2.2

Maybe the version of BSP is not different from yours, but it can still provide some help for your porting.

Q1:

wlan0 is created by your wifi driver. you don't need to modify it.

Q2:

when you configuring linux kernel by typing " make menuconfig ", I think you should have selected "nl80211" , the issue should be generated by "Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0": ".

In addition, the directory "/data/system/wpa_supplicant/wlan0" is given in wifi.c file and Boardconfig.mk file, check them , please!

Regards,

Weidong

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,412件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Raj,

    Refer to the link, please!

Porting BCM4330/BCM43362 WIFI to Android4.2.2

Maybe the version of BSP is not different from yours, but it can still provide some help for your porting.

Q1:

wlan0 is created by your wifi driver. you don't need to modify it.

Q2:

when you configuring linux kernel by typing " make menuconfig ", I think you should have selected "nl80211" , the issue should be generated by "Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0": ".

In addition, the directory "/data/system/wpa_supplicant/wlan0" is given in wifi.c file and Boardconfig.mk file, check them , please!

Regards,

Weidong

0 件の賞賛
返信
3,411件の閲覧回数
ThanarajS
Contributor III

Hi Weidong,

     Thanks Weidong. We cleared that error instead of passing '/data/system/wpa_supplicant/wlan0',we just gave wlan0. Now we were able to see in GUI ( Searching for Wi-Fi networks...) and Wifi enabled.

Regards,

Raj.

Regards,
Thanaraj Subramani
0 件の賞賛
返信