Unable to handle kernel paging request at virtual address ffff00001a9cd000 in i.mx8mm evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to handle kernel paging request at virtual address ffff00001a9cd000 in i.mx8mm evk

Jump to solution
17,744 Views
sreedhar_appala
Contributor IV

Hi,

I am working with i.mx8mm evk and one dsp is interfaced to it. Yocto distribution 4.19.35 imx-warrior.

SAI1 interface connected to serial port of DSP for I2S playback and

SAI5 interface connected to another serial port of DSP for I2S capture.

when i tried to do pass-through test (aplay, followed by arecord alsa utils)

hw_params for playback and capture: channels : 8, format : S32_LE and sampling rate : 48000

The capture starts and i get the paging request error, please find the log below:

root@imx8mmevk:~# ./play32.sh
root@imx8mmevk:~# Playing WAVE 'ref8_32bit.wav' : Signed 32 bit Little Endian, Rate 48000 Hz, Channels 8

root@imx8mmevk:~# ./cap.sh
[ 26.962635] MIC BE: adsp_pcm_be_startup [be_mic_rec]
[ 26.977791] MIC_FE: adsp_pcm_fe_startup [fe_mic_rec]
Recording WAVE 'mic.wav' : [ 26.995513] MIC BE: adsp_pcm_be_hw_params [be_mic_rec] rate 48000 ch 8 bits 32 period 160-4
Signed 32 bit Little Endian, Rate[ 27.007136] MIC BE: adsp_pcm_be_hw_params [be_mic_rec] mclk 24576000 lrck_width 32
48000 Hz, Channels 8
[ 27.020052] MIC BE: adsp_pcm_be_hw_params [be_mic_rec] lrck_inv 0 bck_inv 0
[ 27.038681] MIC_FE: adsp_pcm_fe_hw_params [fe_mic_rec] rate 48000 ch 8 bits 32 period 160-4
[ 27.154868] MIC_FE: buf : 0xf3b7cf0 , hwbuf : 0x1a9c5000 , copy_bytes : 163840
[ 27.169518] Unable to handle kernel paging request at virtual address ffff00001a9cd000
[ 27.177450] Mem abort info:
[ 27.180242] ESR = 0x96000007
[ 27.183318] Exception class = DABT (current EL), IL = 32 bits
[ 27.189254] SET = 0, FnV = 0
[ 27.192307] EA = 0, S1PTW = 0
[ 27.195466] Data abort info:
[ 27.198362] ISV = 0, ISS = 0x00000007
[ 27.202215] CM = 0, WnR = 0
[ 27.205201] swapper pgtable: 4k pages, 48-bit VAs, pgdp = 00000000a64ad819
[ 27.212099] [ffff00001a9cd000] pgd=00000000bdffe803, pud=00000000bdffd803, pmd=00000000b02e7003, pte=0000000000000000
[ 27.222739] Internal error: Oops: 96000007 [#1] PREEMPT SMP
[ 27.228311] Modules linked in: 8021q garp stp mrp qca9377(O) crc32_ce crct10dif_ce galcore(O)
[ 27.236847] Process arecord (pid: 4276, stack limit = 0x00000000444534a6)
[ 27.243635] CPU: 2 PID: 4276 Comm: arecord Tainted: G O 4.19.35-1.1.0+g0f9917c #1
[ 27.252416] Hardware name: FSL i.MX8MM EVK board (DT)
[ 27.257465] pstate: 20000005 (nzCv daif -PAN -UAO)
[ 27.262260] pc : __memcpy_fromio+0x48/0x88
[ 27.266357] lr : copy_to_user_fromio+0xf4/0x108
[ 27.270884] sp : ffff00001a98ba80
[ 27.274196] x29: ffff00001a98ba80 x28: 0000000000000000
[ 27.279507] x27: 0000000000000000 x26: ffff8000752c8880
[ 27.284817] x25: 0000000000000000 x24: ffff80007542d000
[ 27.290128] x23: ffff0000096086c8 x22: ffff00001a9cd000
[ 27.295439] x21: 000000000f3bfcf0 x20: 0000000000000010
[ 27.300749] x19: 0000000000000010 x18: 0000000000000010
[ 27.306059] x17: 0000000000000000 x16: 0000000000000000
[ 27.311370] x15: ffffffffffffffff x14: ffff0000096086c8
[ 27.316680] x13: ffff0000897d0437 x12: ffff0000097d043f
[ 27.316684] x11: ffff000009620000 x10: ffff00001a98b7f0
[ 27.316688] x9 : 00000000ffffffd0 x8 : ffff000008663c28
[ 27.316692] x7 : 5f707364615f3037 x6 : 0000000000000010
[ 27.316696] x5 : 000000000f3bfcf0 x4 : ffff00001a9cd000
[ 27.316700] x3 : ffff00001a98bad8 x2 : 0000000000000010
[ 27.357669] x1 : ffff00001a9cd000 x0 : ffff00001a98bac8
[ 27.362981] Call trace:
[ 27.365428] __memcpy_fromio+0x48/0x88

imx8mmevk kernel: [ 27.222739] Internal error: Oops: 96000007 [#1] PREEMPT SMP

Message from syslogd@imx8mmevk at Tue May 18 07:40:03 2021 ...
imx8mmevk kernel: [ 27.236847] Process arecord (pid: 4276, stack limit = 0x00000000444534a6)
[ 27.369178] adsp_pcm_pcm_copy+0x104/0x200
[ 27.369183] soc_rtdcom_copy_user+0x3c/0x60
[ 27.369189] interleaved_copy+0x54/0x60
[ 27.369197] __snd_pcm_lib_xfer+0x414/0x6c8
[ 27.422797] snd_pcm_common_ioctl+0x570/0xec8
[ 27.427152] snd_pcm_ioctl+0x28/0x40
[ 27.430726] do_vfs_ioctl+0xb8/0x890
[ 27.434299] ksys_ioctl+0x78/0xa8
[ 27.437612] __arm64_sys_ioctl+0x1c/0x28
[ 27.441535] el0_svc_common+0x84/0xf0
[ 27.445195] el0_svc_handler+0x2c/0x80
[ 27.448942] el0_svc+0x8/0xc
[ 27.451823] Code: 927df0c6 910020c6 8b060003 d503201f (f9400085)
[ 27.457916] ---[ end trace 843b67e7e18b29be ]---

Message from syslogd@imx8mmevk at Tue May 18 07:40:03 2021 ...
imx8mmevk kernel: [ 27.451823] Code: 927df0c6 910020c6 8b060003 d503201f (f9400085)
./cap.sh: line 1: 4276 Segmentation fault arecord -D hw:3,0 -f S32_LE -c 8 -r 48000 mic.wav
root@imx8mmevk:~#

 

The page request is failing exactly after 32768 (0x8000) bytes copy. The hwbuf base addr : 0x1a9c5000

paging request failure at ffff00001a9cd000, 0x1a9cd000 - 0x1a9c5000 = 0x8000.

Since the HW is EVK, I am ruling out the DDR issue.

Could you please tell me where i could look at hwbuf allocation for the programmed hardware parameters.

Any pointers and suggestions will definitely help in me in resolving this issue.

Thank you, Sreedhar

0 Kudos
1 Solution
17,704 Views
sreedhar_appala
Contributor IV

Hi Zhiming Liu,

The number of bytes to copy/read is more than the dma buffer (hwbuff) size.

So I am facing the above issue. Now I have controlled the number of bytes to read based on the allocated hwbuf size, and the above issue is resolved.

Thank you, Sreedhar

View solution in original post

0 Kudos
3 Replies
17,734 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

It seem when you use that capture command ,the pointer is beyond the max hardware address. can you attach your test command?

0 Kudos
17,728 Views
sreedhar_appala
Contributor IV

Hi Zhiming Liu,

Please find the test cmd:

play32.sh : aplay -D hw:2,0 ref8_32bit.wav

cap.sh : arecord -D hw:3,0 -f S32_LE -c 8 -r 48000 mic.wav

Thank you, Sreedhar

0 Kudos
17,705 Views
sreedhar_appala
Contributor IV

Hi Zhiming Liu,

The number of bytes to copy/read is more than the dma buffer (hwbuff) size.

So I am facing the above issue. Now I have controlled the number of bytes to read based on the allocated hwbuf size, and the above issue is resolved.

Thank you, Sreedhar

0 Kudos