Unable to handle kernel NULL pointer dereference at virtual address 00000003 - i.MX6Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to handle kernel NULL pointer dereference at virtual address 00000003 - i.MX6Q

1,468 次查看
szymonstepniews
Contributor I

Hi ,

we use this CPU i.MX6Q - on module CM-FX6 from Compulab.

Kernel 3.10.17

When use command "cat /dev/uradom > /dev/null" after few seconds shows errors up

Unable to handle kernel NULL pointer dereference at virtual address 00000003

...

(link to pastebin below with full error description) :

cat /dev/urandom > /dev/null - Pastebin.com

How to solve this problem with kernel error ?

标签 (3)
0 项奖励
回复
1 回复

968 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Szymon

this may be due to ddr errors, for example using incorrect (for other board)

image. Also Kernel 3.10.17 is quite old. One can ask Compulab

support for better last kernel for used board

Welcome to CompuLab Support | CompuLab

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复